STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Use ITCM for dynamic Bitmap (TouchGFX 4.18)

Hello, I'm using an STM32H750 and I need to implement a single small dynamic bitmap, but I have only ITCM RAM available. I read and made all the code from the articlehttps://support.touchgfx.com/docs/development/ui-development/touchgfx-engine-feature...

touchgfx

Can't touchgfx RGB565 images be mixed and displayed My two RGB 565 images overlap and only one can be displayed

Utilisation de la carte GFX01M2 (afficheur+memoire+joystick) avec une carte nucleo 64 STm32303RE

Bonjour à toutes et à tous.C'est la première fois que j'utilise la communauté ST. Pour un projet pour mes étudiants de BTS, je veux mettre en œuvre en C, la carte GFX01M2 (afficheur+mémoire+joystick) de chez ST avec une carte nucléo 64 STm32303RE.J'a...

Profbts by Associate II
  • 7664 Views
  • 3 replies
  • 0 kudos

RGB666

Hi,I am using stm32h753vi 100pin package.I have it set up with touchgfx, and am getting output on my lcd (Raystar RFS520A-AZH-DNG 128x480).I chose this stm32 as space is quite limited, and I don't need RGB888 (I don't think). I have connected it as R...

0693W00000APmEzQAL.jpg 0693W00000APmFEQA1.jpg 0693W00000APmFiQAL.jpg
Cclad.1 by Associate II
  • 9356 Views
  • 8 replies
  • 1 kudos

How to use LibJPEG on STM32?

Hi all,​I build a project with STM32CubeMX and using LibJPEG to decode the JPEG file from SDCard.And now I face a problem ,when it goes to the step 5 - start to decompress, it will stock in that function with no reason and the hardfault descripe like...

0690X00000AqkGJQAZ.png 0690X00000AqkFzQAJ.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.