STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! list layout west

How to put elements in list to the west? I set list direction WEST but it does not working.I found out that its not supported Maybe there is another way to put elements from east to west?

heyo_0-1715664006122.png
heyo by Senior
  • 1739 Views
  • 2 replies
  • 0 kudos

Resolved! touchgfx error

Hi community members !!I’m attempting to open my touchgfx file (.touchgfx file) from the ST32Cube IDE, but I’m running into an error that states, “Value cannot be null. (Parameter ‘path2’)”. I’ve attached a screenshot for reference. This is the first...

touchgfx_error.png
KPeri by Associate II
  • 2001 Views
  • 3 replies
  • 0 kudos

Resolved! TouchGFX Sliding Transitions to screens

Hello,I am using STM32H745 controller with TouchGFX. I wanted to achieve slide transitions such as top to bottom, left to right and right to left for going to other screens. When I slide from top edge to down, slide from right edge to left, slide fro...

ATank.1 by Associate III
  • 3422 Views
  • 5 replies
  • 1 kudos

Resolved! TouchGFX - Library functions used (maths, strings).

Hi all,I currently working on a project using TouchGFX, multiple tasks are using functions from <math.h> which are not re-entrant, so I have them mutex protected. The drivers using these functions are written in C.Does anyone know if the TouchGFX lib...

AMars.4 by Associate III
  • 6942 Views
  • 11 replies
  • 8 kudos

Resolved! Visual bug sometimes after power cycling

Hello,I am developing a TouchGFX application for my STM32H7 MCU using LTDC. Sometimes, after turning the system on, the assets on screen looks "smeared out". Or rather, it looks out of sync or something similar. Restarting the system usually resolves...

TouchGFX_bad.png TouchGFX_good.png
PontusL by Associate III
  • 2540 Views
  • 4 replies
  • 0 kudos

Resolved! TouchGFX: Make Font Bold

Hello, I am trying to make text bold using the TouchGFX Designer. I am using 4.20.0 at the moment.Is this something that is possible?  I am trying to look for options, but I am not having any luck.

KMew by Senior III
  • 2471 Views
  • 3 replies
  • 1 kudos

Text View: double-click adjusts only one column

Dear Gfx Team,Could you please consider changing the following behaviour.When in Text view and double click in any edge, adjust width of all columns - not just the one associated with that edge.Example:Intial widthsDouble click on the boundry... only...

ferro_4-1716376225260.png ferro_6-1716376320963.png ferro_5-1716376274662.png ferro_3-1716376169362.png
ferro by Lead
  • 1357 Views
  • 1 replies
  • 1 kudos

Resolved! GFX use of internal RAM?

I noticed that areas of internal SRAM appear to be used by GFX. I inferred this from a project I am doing with an H745 dual core micro; I set aside a small amount of SRAM4 to be shared between the cores, and I can watch on the debugger as portions of...

VO by Associate III
  • 4021 Views
  • 5 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.