STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! Modal Window from ListLayout

I have created a custom container which includes some text boxes, scrollists labels etc to allow the user to set the parameters for an alarm. I add one of these custom containers to my listlayout in code for each alarm to be set. So the user is prese...

CYBR_0-1716684345138.png
CYBR by Associate II
  • 3190 Views
  • 5 replies
  • 0 kudos

Resolved! Flipping the screen upside down inclusive the buttons

Hello everyone,Hello @Martin KJELDSEN , I have read all the posts in the community, thats with this topic relevant and tried to do the same thing in this post.I could reversed the screen with 180 degree, except the buttons they staying on the origina...

mids400_0-1716554969095.png mids400_1-1716555028340.png
mids400 by Associate III
  • 3001 Views
  • 4 replies
  • 0 kudos

Resolved! How to realize scroll bar effect in ScrollList.

I want to realize a scroll bar in ScrollList.So the scroll bar will work like process bar. And it will tell my user where the current icon is.Is there any clever way to realize it.In addition, can I customize the scroll bar?

Wrend.1 by Senior
  • 8569 Views
  • 12 replies
  • 1 kudos

Resolved! blockCopy function not called with TGFX 4.23.2

Hello,I started a new design based on an STM32H745XI with a 480x272 TFT screen.I have some experience with TouchGFX with a previous design on an STM32H7B3 with the same screen but this development is stucked at the TouchGFX 4.17 revision.My problem i...

PJEN by Senior
  • 2492 Views
  • 3 replies
  • 0 kudos

setup stm32u59 without touchgfx imported example

Hi, I'm using an STM32U5 DK and I'm comfortable with TouchGFX and its code generation features. However, I'm struggling to achieve the same results manually, as there are many changes in both hardware configuration and TouchGFX files. Can anyone guid...

Anassoumi by Associate III
  • 2670 Views
  • 2 replies
  • 0 kudos

Resolved! Setting up and configuring a round display with TouchGFX

Hi,I never worked with STM32 platform. I have to interface a SDI round display with it.I have seen that TouchGFX includes three "parts": TouchGFX Generator, TouchGFX Designer, TouchGFX Engine. But still not sure what each of them does.A couple of que...

Ricko by Senior III
  • 4836 Views
  • 6 replies
  • 5 kudos

Resolved! TouchGFX Password save

Hi all,as I'm new to TouchGFX I'm struggeling on a problem hat does not look difficult at first glance.My problem:On screen_1 there is a Text Area allowes the use to enter a string as input.The entered string is needed on screen_2. As far as I know, ...

HaJott by Associate
  • 3658 Views
  • 2 replies
  • 1 kudos

Resolved! NUCLEO-GFX01M2 Initialization error

I'm running the following git source on the NUCLEO-G071RB with NUCLEO-GFX01M2.GitHub - lvgl/lv_port_stm_nucleo_g071rb: LVGL ported to ST's NUCLEO G071RB boardBut, I got an error at the cursor location from the attached figure (LCD Error 1.png).The re...

LCD Error 1.png 시험 Setup.jpg
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.