STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Resolved! How TouchGFX access the non memory map area?

Hi there,I have a GUI demo of TouchGFX on my STM32F429BI board, and it works well when the image is stored in the inner flash.But when I stored the image external Nand-flash by FMC, it could NOT work.It's said that the Nand-flash extended by FMC can'...

Junde by Senior III
  • 2015 Views
  • 2 replies
  • 0 kudos

Resolved! TouchGFX as a standalone application

Hello,I wanted to use the TouchGFX as a standalone simulator application which simulates a hardware.  Following requirements should be fullfilled,1. TouchGFX should be able to compile an existing FreeRTOS application on PC only and run a frontend GUI...

ATank.1 by Associate III
  • 2546 Views
  • 3 replies
  • 1 kudos

Stm32F407 with Monochrome Custom LCD

Hi All,Actually, I've just started using stm32f4 discovery board. I'm trying to make a Stm32project with custom based monochrome LCD. So, Is it possible to work it using TouchGFX? I have tried to build an empty project in the IAR Workbench, but it fa...

azMikro_0-1715855000676.png
azMikro by Associate II
  • 4108 Views
  • 5 replies
  • 2 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.