STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Rotate screen 180 degrees

I would like to rotate my screen 180 degrees, I know that Touchgfx does not support this option but it is possible to do so by modifying the internal registers of the display controller.In my case the display has a resolution of 480x272 and the contr...

cb.7 by Associate III
  • 1902 Views
  • 2 replies
  • 0 kudos

MIPI DSI Clock not starting

I've configured a skeleton CubeMX project upon which ive enabled the DMA2D, DSIHOST and LTDC IPs for a custom board. The boards test okay, access to the MCU, programming, sane registers, but upon flashing the CubeMX generated firmware the DSI clock ...

DAllo by Associate II
  • 3094 Views
  • 3 replies
  • 0 kudos

Resolved! Question about the TouchGFX interface

Hi, CARHER  I just want to know what is the software you show in the picture? Where to download it? thank you. post created based on a command posted on an old thread. here is the picture mentioned by the customer:     

STTwo32_0-1738682566316.png
rhine1012 by Associate II
  • 1005 Views
  • 1 replies
  • 0 kudos

TouchGFX_STM32H7B3I-DK_Build Errors

Dear Sir, Hardware: STM32H7B3I-DKSoftware: STM32MX 6.13.0 / STM32CubeIDE 1.17.0 / TouchGFX 4.24.1/ STM32Cube_FW_H7_V1.12.0 Start the project from TouchGFX, and then refer to STM32 Graphics Workshop (STM32H7BWorkshop2020_labs12345), to develop the det...

EY1_0-1738140512229.png EY1_1-1738140572073.png EY1_2-1738140722305.png
EY1 by Associate II
  • 6328 Views
  • 8 replies
  • 4 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.