2026-03-23 4:35 AM
On an STM32H563, I am trying to write the OBkey1 data.
I have successfully set the product state to provisioning (0x17) with:
FLASH_OBProgramInitTypeDef optionBytes;
HAL_FLASHEx_OBGetConfig(&optionBytes);
HAL_FLASH_Unlock();
HAL_FLASH_OB_Unlock();
optionBytes.OptionType = OPTIONBYTE_PROD_STATE;
optionBytes.ProductState = OB_PROD_STATE_PROVISIONING;
HAL_FLASHEx_OBProgram(&optionBytes);
HAL_FLASH_OB_Launch();
HAL_FLASH_OB_Lock();Now, when I try to write too OBKey1 with:
uint32_t dataAddr = 0x20050000;
memcpy ((void*)dataAddr, source, 0x60);
RSSLIB_DataProvisioningConf_t * pConfig = (RSSLIB_DataProvisioningConf_t *)0x20050100;
pConfig->pSource = (uint32_t*)dataAddr;
pConfig->pDestination = (uint32_t*)0xffd0100;
pConfig->Size = 0x60;
pConfig->DoEncryption = 0xCACA0AA0U;
pConfig->Crc = 0;
HAL_FLASHEx_OBK_Unlock();
provisioningResult = RSSLIB_PFUNC->NSC.DataProvisioning(pConfig);
HAL_FLASHEx_OBK_Lock();The call to DataProvisioning() causes a hard fault.
I am aware that the checksum (0) is currently incorrect but the reference manual suggests that should return error code 0xF5F58080U .
My source data is copied to a buffer in SRAM3 (0x20050000) as specified in the RM - I also have the config struct in SRAM3 (I'm not sure if that is needed or not but it doesn't seem to make a difference).
I would be grateful for any suggestions about what I am doing wrong. I have noticed that SCB->BFSR_S-> IBUSERR is set to 1 but nothing in BFSR_NS which seems strange because I have Trust Zone disabled and understood that means everything should be Non Secure.
2026-03-26 3:36 AM
Hello ,
you cannot use the DataProvisioning service when TrustZone is disabled because it is a non secure callable service.
Now, as you use a non crypto device (STM32H563), you can just write the data directly in the OBK with your firmware.
I provided an example for crypto device here that you can use as example. You will need to remove the encryption part.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.