2024-09-23 8:27 AM - edited 2024-09-23 8:28 AM
Hello,
I've been working on Provisioning my STM32H563 product and after 3 weeks of not touching the project, I am unable to perform Full Regression or Debug Authentication on my password-provisioned Nucleo Board. I tried using the generated bash scripts from CubeIDE/MX (which are using STM32_Programmer_CLI) and also STM32CubeProgrammer GUI.
I remember before the vacation, I could open and close the Board at will. I always used the same password(.bin).
Provisioning always happened using the generated provisioning.sh script.
Here is the Output of STM32CubeProgrammer (I found it has more info than dbg_auth.sh), after trying Discovery and Full Regression:
------------------------------------------------------------------
What could be the issue here?
Thank you and best regards,
Stefan
2024-09-24 7:01 AM
Hello @beartronics ,
are you sure you are selecting the same key that you used before make sure the path tp the key is correct maybe it is a naming issue.
also did you make sure that you had an application running in the non-secure world if you have TZ enabled.
make sure you check and follow the recommended steps in the related WIKI series:
Category:How to start with DA on STM32H5 - stm32mcu
Regards
2024-09-25 6:46 AM
Hello @STea ,
thank you for the reply. Sorry for duplicating this post - this one here was originally marked as spam, which is why I made another one:
https://community.st.com/t5/stm32-mcus-security/stm32h563-unable-to-regress-or-debug-authenticate
Unfortunately, your suggestions do not apply to my problem. Thanks anyways!
Best regards,
Stefan
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.