2021-12-29 1:37 AM
The size of system memory on STM32H743 is 2 sectors of 128KB each.
What is the size of the option bytes block?
2021-12-29 6:45 AM
Option bytes are not directly accessible. So in one sense they don't have a size as they don't exist anywhere in the memory map.
You can only modify them indirectly through the register interface shown in the FLASH section of the RM, which gives you access to portions of 8x 32-bit words.
2021-12-29 12:32 PM
Thanks.
Is it possible to write into System memory region from user flash regions in RDP level 0 ?
2021-12-29 12:39 PM
2021-12-29 8:29 PM
Is possible while running form Flash in RDP level 0 to:
Is it possible?
I know that if RDP level 2 is applied you can only boot into user flash or into System Memory.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.