2022-10-08 5:46 AM
Hello,
I am trying to flashing customized SBSFU_UserApp.bin of 1_Image application from BSFU example project on STM32H7B3I-DK.
I am getting error when the application is booting. The error is:
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Hardware reset!
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
No valid FW found in the active slots nor new FW to be installed
Waiting for the local download to start...
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
File> Transfer> YMODEM> Send ...............
The reference 1_Image of STM32H7B3I-DK is working fine.
I am adding a new crypto scheme in this application. I have not change any address in the Linker_Common files. I am setting the application in development mode through app_sfu.h fie. The compilation of 3 applications, prebuild and postbuild scripts is successfully done.
I am trying to read back the flash of STM32 and I find the address 0x08010400 is empty, however the SBSFU application and my customized active image header is visible in the respective flash area.
I have added some debug log in postbuild script and it seems like the postbuild is working fine.
I am not able to understand the reason for not merging of UserApp in big binary.
Please help me to fixed this issue.
Thanks,
Ikbal
2022-10-10 1:02 AM
Hi @Ikbal,
you wrote that the only change you've done is the crypto scheme added? Maybe you could try to compare the map files of the apps to see the differences - there may be a need for linker file alteration after all. Or maybe try to undo some changes to see which caused the failure.
Also when you try to upload the sfb file to the device, does at least that work?
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-10 6:16 AM
Hi JHOUD,
Thanks for the response. I tried to follow the process mentioned.
A) I tried to upload the sfb file and I am getting error related to header authentication. The error log is show in below:
======================================================================
= (C) COPYRIGHT 2017 STMicroelectronics =
= =
= Secure Boot and Secure Firmware Update =
======================================================================
= [SBOOT] SECURE ENGINE INITIALIZATION SUCCESSFUL
= [SBOOT] STATE: CHECK STATUS ON RESET
INFO: A Reboot has been triggered by a Hardware reset!
= [SBOOT] STATE: CHECK NEW FIRMWARE TO DOWNLOAD
= [SBOOT] STATE: CHECK USER FW STATUS
No valid FW found in the active slots nor new FW to be installed
Waiting for the local download to start...
= [SBOOT] STATE: DOWNLOAD NEW USER FIRMWARE
File> Transfer> YMODEM> Send .
Fw header authentication error
= [SBOOT] STATE: HANDLE CRITICAL FAILURE
= [SBOOT] STATE: REBOOT STATE MACHINE
========= End of Execution ==========
= [SBOOT] RuntimeProtections: 0
= [SBOOT] System Security Check successfully passed. Starting...As per my understanding the error is coming during header authentication check upon start of download sfb app. Please note that earlier when I tried to flash the SBSFU_UserApp.bin , the SBDFU App & the header were successfully written to the flash but the user application is not written to flash.
I have a question regarding when the header is written for the very first time. Is any header authentication performed at that time ?.
I feel that header authentication should not be performed at the very first time as the newly written SBSFU & then user application have to be tested and debugged.
.
Please confirm if my understanding is correct,.
B) I have disassembled the SBSFU_UserApp.bin using $ hexdump -C SBSFU_UserApp.bin and I am able to see the content at 0x00010400 address of the dump. But when I read back the same address directly from the flash there is nothing at that location. Its look like flashing of the SBSFU_UserApp.bin is happening partially as mentioned in A) above.
It appears that i have either missed something or done something wrong while making post-build scripts. Please let me know the likely area in post-build script where this could have happene whereby while full code is being built properly but not flashed completely.
C) The changes I have done in se_crypto_bootloader.c are for adding "new crypto" support and in the length of SE_HEADER_SIGN_LEN micro for the "new crypto" sign length.
I have compared the map files of the STM32H7B3I-DK ECC application and my application with respect to memory configuration and linker script & memory map, but there are no differences. The log is attached in the next answer.
Please suggest what else I can check to solve the problem.
Thanks & Best Regards,
Ikbal
2022-10-10 6:19 AM
Hi,
I am attaching the same logs below:
Memory Configuration
Name Origin Length Attributes
SE_Entry_Secure_ROM_Region 0x0000000008000400 0x0000000000000200 xr
SE_Key_region_ROM 0x0000000008000600 0x0000000000000300 xr
SE_Startup_region_ROM 0x0000000008000900 0x0000000000000100 xr
SE_ROM_region 0x0000000008000a00 0x0000000000005600 xr
SE_IF_region_ROM 0x0000000008006000 0x0000000000000900 xr
SB_HDP_ROM_region 0x0000000008006900 0x0000000000000100 xr
SB_ROM_region 0x0000000008006a00 0x0000000000009600 xr
SE_RAM_region 0x0000000020000400 0x0000000000000c00 xrw
SB_HDP_Code_RAM_region 0x0000000020001000 0x0000000000000100 xrw
SB_RAM_region 0x0000000020001100 0x000000000001ef00 xrw
*default* 0x0000000000000000 0xffffffffffffffff
Linker script and memory map
0x0000000000000000 _Min_Heap_Size = 0x0
0x0000000000000000 _Min_Stack_Size = 0x0
0x0000000008010000 __ICFEDIT_SLOT_Active_1_start__ = 0x8010000
0x00000000081fffff __ICFEDIT_SLOT_Active_1_end__ = 0x81fffff
0x0000000008010000 __ICFEDIT_SLOT_Active_1_header__ = __ICFEDIT_SLOT_Active_1_start__
0x0000000000000000 __ICFEDIT_SLOT_Active_2_header__ = 0x0
0x0000000000000000 __ICFEDIT_SLOT_Active_2_start__ = 0x0
0x0000000000000000 __ICFEDIT_SLOT_Active_2_end__ = 0x0
0x0000000000000000 __ICFEDIT_SLOT_Active_3_header__ = 0x0
0x0000000000000000 __ICFEDIT_SLOT_Active_3_start__ = 0x0
0x0000000000000000 __ICFEDIT_SLOT_Active_3_end__ = 0x0
0x0000000000000400 VECTOR_SIZE = 0x400
0x0000000008000400 __ICFEDIT_SE_Code_region_ROM_start__ = (0x8000000 + VECTOR_SIZE)
0x0000000008000400 __ICFEDIT_SE_CallGate_region_ROM_start__ = __ICFEDIT_SE_Code_region_ROM_start__
0x00000000080005ff __ICFEDIT_SE_CallGate_region_ROM_end__ = (__ICFEDIT_SE_Code_region_ROM_start__ + 0x1ff)
0x0000000008000600 __ICFEDIT_SE_Key_region_ROM_start__ = (__ICFEDIT_SE_CallGate_region_ROM_end__ + 0x1)
0x00000000080008ff __ICFEDIT_SE_Key_region_ROM_end__ = (__ICFEDIT_SE_Key_region_ROM_start__ + 0x2ff)
0x0000000008000900 __ICFEDIT_SE_Startup_region_ROM_start__ = (__ICFEDIT_SE_Key_region_ROM_end__ + 0x1)
0x0000000008000a00 __ICFEDIT_SE_Code_nokey_region_ROM_start__ = (__ICFEDIT_SE_Startup_region_ROM_start__ + 0x100)
0x0000000008005fff __ICFEDIT_SE_Code_region_ROM_end__ = 0x8005fff
0x0000000008006000 __ICFEDIT_SE_IF_region_ROM_start__ = 0x8006000
0x00000000080068ff __ICFEDIT_SE_IF_region_ROM_end__ = (__ICFEDIT_SE_IF_region_ROM_start__ + 0x8ff)
0x0000000008006900 __ICFEDIT_SB_HDP_region_ROM_start__ = (__ICFEDIT_SE_IF_region_ROM_end__ + 0x1)
0x00000000080069ff __ICFEDIT_SB_HDP_region_ROM_end__ = (__ICFEDIT_SB_HDP_region_ROM_start__ + 0xff)
0x0000000008006a00 __ICFEDIT_SB_region_ROM_start__ = (__ICFEDIT_SB_HDP_region_ROM_end__ + 0x1)
0x000000000800ffff __ICFEDIT_SB_region_ROM_end__ = 0x800ffff
0x0000000000000200 SE_Entry_Secure_ROM_Region_Length = ((__ICFEDIT_SE_CallGate_region_ROM_end__ - __ICFEDIT_SE_CallGate_region_ROM_start__) + 0x1)
0x0000000000000300 SE_Key_region_ROM_Length = ((__ICFEDIT_SE_Key_region_ROM_end__ - __ICFEDIT_SE_Key_region_ROM_start__) + 0x1)
0x0000000000000100 SE_Startup_region_ROM_Length = (__ICFEDIT_SE_Code_nokey_region_ROM_start__ - __ICFEDIT_SE_Startup_region_ROM_start__)
0x0000000000005600 SE_ROM_region_Length = ((__ICFEDIT_SE_Code_region_ROM_end__ - __ICFEDIT_SE_Code_nokey_region_ROM_start__) + 0x1)
0x0000000000000900 SE_IF_region_ROM_Length = ((__ICFEDIT_SE_IF_region_ROM_end__ - __ICFEDIT_SE_IF_region_ROM_start__) + 0x1)
0x0000000000000100 SB_HDP_ROM_region_Length = ((__ICFEDIT_SB_HDP_region_ROM_end__ - __ICFEDIT_SB_HDP_region_ROM_start__) + 0x1)
0x0000000000009600 SB_ROM_region_Length = ((__ICFEDIT_SB_region_ROM_end__ - __ICFEDIT_SB_region_ROM_start__) + 0x1)
0x0000000020000000 __ICFEDIT_SE_region_RAM_start__ = 0x20000000
0x0000000020000400 __ICFEDIT_SE_region_RAM_stack_top__ = 0x20000400
0x0000000020000fff __ICFEDIT_SE_region_RAM_end__ = 0x20000fff
0x0000000020001000 __ICFEDIT_SB_HDP_Code_region_RAM_start__ = (__ICFEDIT_SE_region_RAM_end__ + 0x1)
0x00000000200010ff __ICFEDIT_SB_HDP_Code_region_RAM_end__ = (__ICFEDIT_SB_HDP_Code_region_RAM_start__ + 0xff)
0x0000000020001100 __ICFEDIT_SB_region_RAM_start__ = (__ICFEDIT_SB_HDP_Code_region_RAM_end__ + 0x1)
0x000000002001ffff __ICFEDIT_SB_region_RAM_end__ = 0x2001ffff
0x0000000000000c00 SE_RAM_region_Length = ((__ICFEDIT_SE_region_RAM_end__ - __ICFEDIT_SE_region_RAM_stack_top__) + 0x1)
0x0000000000000100 SB_HDP_CODE_RAM_region_Length = ((__ICFEDIT_SB_HDP_Code_region_RAM_end__ - __ICFEDIT_SB_HDP_Code_region_RAM_start__) + 0x1)
0x000000000001ef00 SB_RAM_region_Length = ((__ICFEDIT_SB_region_RAM_end__ - __ICFEDIT_SB_region_RAM_start__) + 0x1)
2022-10-10 6:22 AM
Hi,
Some differences were also there and log is given below.
.text.SE_CRYPTO_Authenticate_Metadata
0x0000000008000bf0 0xf0 ./Application/User/se_crypto_bootloader.o
0x0000000008000bf0 SE_CRYPTO_Authenticate_Metadata
.text.__NVIC_SystemReset
0x0000000008000ce0 0x24 ./Application/User/se_low_level.o
.text.SE_LL_GetSector
0x0000000008000d04 0x34 ./Application/User/se_low_level.o
.text.SE_LL_CRC_Config
0x0000000008000d38 0x38 ./Application/User/se_low_level.o
0x0000000008000d38 SE_LL_CRC_Config
.text.SE_LL_FLASH_Erase
0x0000000008000d70 0xb0 ./Application/User/se_low_level.o
0x0000000008000d70 SE_LL_FLASH_Erase
.text.SE_LL_FLASH_Write
0x0000000008000e20 0x54 ./Application/User/se_low_level.o
0x0000000008000e20 SE_LL_FLASH_Write
.text.SE_LL_FLASH_Read
0x0000000008000e74 0x58 ./Application/User/se_low_level.o
0x0000000008000e74 SE_LL_FLASH_Read
.text.SE_LL_Buffer_in_ram
0x0000000008000ecc 0x30 ./Application/User/se_low_level.o
0x0000000008000ecc SE_LL_Buffer_in_ram
.text.SE_LL_Buffer_in_SBSFU_ram
0x0000000008000efc 0x30 ./Application/User/se_low_level.o
0x0000000008000efc SE_LL_Buffer_in_SBSFU_ram
.text.SE_LL_Buffer_part_of_SE_ram
0x0000000008000f2c 0x38 ./Application/User/se_low_level.o
0x0000000008000f2c SE_LL_Buffer_part_of_SE_ram
.text.SE_LL_CORE_Cleanup
0x0000000008000f64 0x4 ./Application/User/se_low_level.o
0x0000000008000f64 SE_LL_CORE_Cleanup
.text.SE_LL_Lock_Keys
0x0000000008000f68 0x8 ./Application/User/se_low_level.o
0x0000000008000f68 SE_LL_Lock_Keys
.text.HAL_CRC_MspInit
0x0000000008000f70 0x2 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_crc.o
0x0000000008000f70 HAL_CRC_MspInit
*fill* 0x0000000008000f72 0x2
.text.HAL_CRC_Init
0x0000000008000f74 0x74 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_crc.o
0x0000000008000f74 HAL_CRC_Init
.text.HAL_CRCEx_Polynomial_Set
0x0000000008000fe8 0x48 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_crc_ex.o
0x0000000008000fe8 HAL_CRCEx_Polynomial_Set
.text.HAL_FLASH_Unlock
0x0000000008001030 0x4c ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash.o
0x0000000008001030 HAL_FLASH_Unlock
.text.HAL_FLASH_Lock
0x000000000800107c 0x30 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash.o
0x000000000800107c HAL_FLASH_Lock
.text.FLASH_WaitForLastOperation
0x00000000080010ac 0xc0 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash.o
0x00000000080010ac FLASH_WaitForLastOperation
.text.HAL_FLASH_Program
0x000000000800116c 0xec ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash.o
0x000000000800116c HAL_FLASH_Program
.text.FLASH_MassErase.constprop.0
0x0000000008001258 0x3c ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash_ex.o
.text.FLASH_Erase_Sector
0x0000000008001294 0x44 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash_ex.o
0x0000000008001294 FLASH_Erase_Sector
.text.HAL_FLASHEx_Erase
0x00000000080012d8 0x120 ./Drivers/STM32H7xx_HAL_Driver/stm32h7xx_hal_flash_ex.o
0x00000000080012d8 HAL_FLASHEx_Erase
.text.__NVIC_SystemReset
0x00000000080013f8 0x24 ./Middlewares/STM32_Secure_Engine/se_callgate.o
.text.SE_CallGateService
0x000000000800141c 0x4d0 ./Middlewares/STM32_Secure_Engine/se_callgate.o
0x000000000800141c SE_CallGateService
.text.SE_IMG_Write
0x00000000080018ec 0x2c ./Middlewares/STM32_Secure_Engine/se_fwimg.o
0x00000000080018ec SE_IMG_Write
.text.SE_IMG_Read
0x0000000008001918 0x2c ./Middlewares/STM32_Secure_Engine/se_fwimg.o
0x0000000008001918 SE_IMG_Read
.text.SE_IMG_Erase
0x0000000008001944 0x30 ./Middlewares/STM32_Secure_Engine/se_fwimg.o
0x0000000008001944 SE_IMG_Erase
.text.SE_APPLI_GetActiveFwInfo
0x0000000008001974 0x40 ./Middlewares/STM32_Secure_Engine/se_user_application.o
0x0000000008001974 SE_APPLI_GetActiveFwInfo
.text.SE_SetSystemCoreClock
0x00000000080019b4 0xc ./Middlewares/STM32_Secure_Engine/se_utils.o
0x00000000080019b4 SE_SetSystemCoreClock
.text.HAL_GetTick
0x00000000080019c0 0x40 ./Middlewares/STM32_Secure_Engine/se_utils.o
0x00000000080019c0 HAL_GetTick
.text.SHA256Transform
0x0000000008001a00 0x278 ../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32H7A3/Lib\STM32CryptographicV3.1.3_CM7_GCC.a(crypto.o)
.text.SHA256Update
0x0000000008001c78 0x8e ../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32H7A3/Lib\STM32CryptographicV3.1.3_CM7_GCC.a(crypto.o)
0x0000000008001c78 SHA256Update
.text.SHA256_Append
0x0000000008001d06 0x26 ../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32H7A3/Lib\STM32CryptographicV3.1.3_CM7_GCC.a(crypto.o)
0x0000000008001d06 SHA256_Append
.text.SHA256Init
0x0000000008001d2c 0x50 ../../../../../../../Middlewares/ST/STM32_Cryptographic/Fw_Crypto/STM32H7A3/Lib\STM32CryptographicV3.1.3_CM7_GCC.a(crypto.o)
There were differences prior during compile time which are due to different crypto schemes.
2022-10-11 2:56 AM
Hi @Ikbal,
there is no obvious problem in the memory mapping, I see.
I still don't know what's the change you did in the cryptography scheme.
Where did you configure the change? in app_sfu.h ? There you can try also disabling some checks and protections for debug purposes.
I should probably also highlight the existence of AN5056 and UM2262 where you may find some tips regarding the cryptography scheme swap in the project.
BR,
J
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-10-11 4:28 AM
Dear JHOUD,
Thank you for the update.
I tried to add RSA signing and verification in place of ECDSA. I followed the AN5056 section 7.1 for adding new crypto scheme but with following modifications:.
Please let me know if I can live without scheme name as detailed above as it would lots of changes. If name change is a must, please let me know the reason for such change,
Further, in app_sfu.h, I have disables all the protection by enabling SECBOOT_DISABLE_SECURITY_IPS.
Thanks & Best Regards,
Ikbal
2022-10-11 11:48 PM
Dear JHOUD,
I able to find the reason of the error. The error is because of Header signature verification failure in slot SLOT_ACTIVE_1.
Now, I want to debug my changes in se_crypto_bootloader.c file of SECoreBin project. I tried to add TRACE same a SBSFU app and printf API's for adding debug messages but I am getting compile time error.
I am using STM32Cube IDE and compiling the applications as per the order maintain in the readme of the STM32H7B3I-DK 1_Image demo project.
I want to know, what is the proper debug mechanism for SECoreBin application? How can I enable debug mode of this application?
Thanks & Best Regards,
Ikbal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.