STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32H735AGI6 RNG non working

the function MX_RNG_Init failsHAL_RNG_Init returns t.o.: while (HAL_IS_BIT_SET(hrng->Instance->CR, RNG_CR_CONDRST)) {  if ((HAL_GetTick() - tickstart) > RNG_TIMEOUT_VALUE)  {   /* New check to avoid false timeout detection in case of preemption */   ...

mzenn.280 by Associate II
  • 2631 Views
  • 3 replies
  • 0 kudos

Resolved! Best approach to security with STM32H757

I am using an STM32H757. I understand how, using the TrustedPackageCreator and an HSM, I can supply our manufactures with an encrypted version of the firmware and limit the number of product instances they can produce. My question is, when the produc...

GRoss.5 by Associate II
  • 1462 Views
  • 1 replies
  • 0 kudos

AES CCM encryption with HW AES module

Hello,I am trying yo implement the HW encryption acceleration on a STM32F423CH for AED CCM Mode. I tried to implement on the first place the CTR encryption mode but it seems to me that the example provided in the NIST Special Publication 800-38A cann...

0693W00000QKNQVQA5.png 0693W00000QKNVQQA5.png 0693W00000QKMq9QAH.png
MSaez.1 by Associate II
  • 2301 Views
  • 1 replies
  • 0 kudos

Resolved! Flash SBSFU application on STM32H7B3I-DK board

Hello,I am trying to flashing SBSFU application on the STM32H7B3I-DK board using STM32Cube Programmer. I am using STM32H7B3I-DK 1_Image example project from SRM32CubeExpansion_SBSFU_V2.6.1. The board is working fine in the first boot and all the jump...

Ikbal by Associate II
  • 5616 Views
  • 8 replies
  • 0 kudos

Is CRC-7 X7+X3+X0 supported by STM32L4R9

I shall just write a function in software but I would be interested to know if it is supported or not by the CRC peripheral hardware.STM32 cube MX configurator does not allow you to choose X7 for the 7bit (8 term) polynomial described on page 21 of t...

Kevlar700 by Associate III
  • 2905 Views
  • 5 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.