2025-09-15 2:30 AM
Hi teams,
CPU: STM32U0
Current RDP level: Level 1
OEM1 RDP lock: Enabled.
I had set the 128bit OEM1 key to the OEM key registers [FLASH_OEM1KEYWyR ]accordingly, and the written OEM1 key values was verified using their CRC values by reading OEM1KEYCRC register.
Now I am trying to make the regression from level 1 to level 0 according to the user manual description [section: 3.5.1 FLASH read protection (RDP)].
But the operation was failed using my source code. Which is attached below
#define STM32U0_DBGMCU_BASE 0x40015800 // Accessible to the software via the APB access port AP0
#define STM32U0_DBGMCU_DBG_AUTH_HOST (STM32U0_DBGMCU_BASE + 0x100) // Debug authentication mailbox host register
Could you please clarify the following doubts,
1. The unlock sequence says, debug access port 1 has to be used for programming the 128-bit OEM1 key in the DBGMCU_DBG_AUTH_HOST register,
but when I checked the DBGMCU_DBG_AUTH_HOST register base, it says
So, what is the base address for DBGMCU_DBG_AUTH_HOST register and which AP should be selected during OEM key write process.
2. After connecting the target from the following settings via STM32 Cube programmer. I have tried to change RDP level using secure programming page.
What could be the reason behind this?
3. If I select the AP to 1, target connection is not feasible and the following error prompt was occurred.
Right now the flash memory is not accessible, please let me know how can I recover from this issue.
Thanks
Akhil
2025-11-13 12:05 PM
Hello,
I made a test on a Nucleo U083RC.
It looks like you need to use ap=1 to provide the key.
Then to set RDP=0xAA, you need to use ap=0
Providing the password:. Here ap=0 and ap=1 both work
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG ap=0 -lockRDP1 0x12345678 0x12345678 0x12345678 0x12345678
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF373857343143073059
ST-LINK FW : V2J46M31
Board : NUCLEO-U083RC
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x489
Revision ID : Rev A
Device name : STM32U0xx
Flash size : 256 KBytes (default)
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xD0
Debug in Low Power mode enabled
Lock RDP1 password successfully done
Set RDP=0xBB:
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob RDP=0xBB
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF373857343143073059
ST-LINK FW : V2J46M31
Board : NUCLEO-U083RC
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x489
Revision ID : Rev A
Device name : STM32U0xx
Flash size : 256 KBytes (default)
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xD0
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
PROGRAMMING OPTION BYTES AREA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
Reconnecting...
Reconnected !
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTE PROGRAMMING VERIFICATION:
Option Bytes successfully programmed
Time elapsed during option Bytes configuration: 00:00:02.215
RDP 1 unlock with ap=1:
C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin>STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG ap=1 -unlockRDP1 0x12345678 0x12345678 0x12345678 0x12345678
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF373857343143073059
ST-LINK FW : V2J46M31
Board : NUCLEO-U083RC
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x489
Revision ID : Rev A
ST-LINK SN : 066FFF373857343143073059
ST-LINK FW : V2J46M31
Board : NUCLEO-U083RC
Voltage : 3.23V
Unlock RDP1 password successfully done
SWD freq : 1800 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x489
Revision ID : Rev A
Device name : STM32U0xx
Flash size : 256 KBytes (default)
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0x0
Debug in Low Power mode enabled
Regression with ap=0 or without specifying ap:
STM32_Programmer_CLI.exe -c port=SWD mode=HOTPLUG -ob RDP=0xAA
-------------------------------------------------------------------
STM32CubeProgrammer v2.20.0
-------------------------------------------------------------------
ST-LINK SN : 066FFF373857343143073059
ST-LINK FW : V2J46M31
Board : NUCLEO-U083RC
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Hot Plug
Reset mode : Software reset
Device ID : 0x489
Revision ID : Rev A
Device name : STM32U0xx
Flash size : 256 KBytes (default)
Device type : MCU
Device CPU : Cortex-M0+
BL Version : 0xD0
Debug in Low Power mode enabled
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
PROGRAMMING OPTION BYTES AREA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
Reconnecting...
Reconnected !
UPLOADING OPTION BYTES DATA ...
Bank : 0x00
Address : 0x40022020
Size : 100 Bytes
██████████████████████████████████████████████████ 100%
OPTION BYTE PROGRAMMING VERIFICATION:
Option Bytes successfully programmed
Time elapsed during option Bytes configuration: 00:00:02.222
I hope this will help
Best regards
Jocelyn
2025-11-14 1:16 AM
Many thanks Jocelyn for the quick feedback!
On a new board, following the steps you described is so far OK. Back at level 0, I can neither flash nor erase the board any more, even though I see "RDP=AA", "OEM1 lock not active" and the memory contents can be read out normally. Can you reproduce this on the Nucleo? This is not systematic, it also works sometimes!
Other thoughts:
- At step 3 (RDP 1 unlock with ap=1), provisioning a wrong password yields "Unlock RDP1 password successfully done". Is this normal?
- Repeating step 1 (Providing the password) to a board with "RDP=BB" also seems to work! I'd expect an error in this case. Is this normal?
- Changing level may fail (even though I executed several time the exact same script), in this case RDP=0, which seems to indicate an option byte corruption. Is there any way to save the board in this case?
The whole thing looks rather unstable to me. Does ST have for example a kind of unit test with a batch repeating the whole process (flash / verify / set PW / set RDP1 / unlock / set RDP0 / read / re-flash, etc.) ?
Thanks again!
2025-11-17 9:51 AM
Using the STM32CubeProgrammer v2.20.0 targeting the STM32U031 RDP 1 unlock with ap=1 with wrong password states command successful. Does not seem differential between correct and incorrect password.
The unlock sequence does work with correct password and applying OPTSRT.
Then disconnecting and reconnecting using Access port 0 then setting to RDP=0 "AA".
The problem relating to this is the password.
If a use for example a password of 0xAA55AA55, 0xAA55AA55, 0xAA55AA55, 0xAA55AA55 or
0x11111111, 0x22222222, 0x33333333, 0x44444444 can be unlocked successfully.
However using a more varied password 0x436F6465, 0x20456E74, 0x72207938, 0x36382031 it will not unlock successfully. I have not inspected the SWD output to determine if the password is set correctly and matching the entered password.
2025-11-24 8:58 AM
Hello,
I made one more test. What I could see:
You need to use ap=1 in the command only to provide the password when device is in RDP1.
If you use ap=1 to set the password, programmer returns ok but password is not actually set.
So, when changing the password, I would suggest first disabling the password (I used GUI Disable password) and then provide new password. You can then double check password is active with same GUI.
I didn't have issue flashing the target after regression.
I used the GPIO toggle example to check firmware was running find. So, after setting RDP1, I power on reset the board to make the led blink again.
Then I provide the password with ap=1, then -ob RDP=0xAA on another command line.
Never had any issue.
The result of -unlockRDP will always be success. You can only check password provide is the good one by performing the regression. If it works it means password was ok
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.