2025-11-11 8:29 AM - edited 2025-11-11 8:36 AM
Hi
I am implementing the ECDSA-P256 signing for a payload.
I have checked the example code https://github.com/STMicroelectronics/STM32CubeU3/tree/main/Projects/NUCLEO-U385RG-Q/Examples/CCB/CCB_Protected_ECDSA_Signature
The example code shows that the software has an access to the private-key. Would it be possible to generate a private key using RNG which software/processor can not see and which can be used by the CCB to compute a signature. The same key can be used to get public-key. can I use this API HAL_CCB_ECDSA_GenerateWrapPrivateKey(). Would this key be persistence across reboot or do I need to store the wrapped key?
2025-11-12 10:06 AM
Hello @SAMINA ,
I guess you are looking for this example:
It is using HAL_CCB_ECDSA_GenerateWrapPrivateKey(). (behind mbedTLS PSA API)
This give you an example how this is connected to flash storage through storage_interface.c implementing psa storage api.
This is very simple example, you will need to adapt it to your needs
Best regards
Jocelyn
2025-11-14 4:38 AM - edited 2025-11-14 7:00 AM
@Jocelyn RICARD
Thanks for the input. I am evaluating the use of Zephyr OS for the selected STM32U385 processor.
I have the similar requirements to
1. Get a public key from the wrapped private key.
2. Sign the payload with the private key.
I would like to use hardware crypto from STM323U3 to do so.
I have created a sample that uses mbedTLS software driver for performing ECDSA signature. I would like to use STM32's hardware crypto backend to perform the signing. How can I do that? Please find the attached example.
I am using Zephyr version v4.3.0-rc1-160-g0f5e03f1fcba.
zephyrproject/modules/hal/stm32 points to the commit 55e159704b02ec4e7b4f0a88735044bee92c25c2 from https://github.com/zephyrproject-rtos/hal_stm32
One can compile the code using following command
# assumed that ENV is sourced. if not source <PATH_TO_ZEPHYR_PROJECT_DIR>/venv/bin/activate
cd <PATH_TO_ZEPHYR_PROJECT_DIR>/zephyr
#compile
west build --pristine --board nucleo_u385rg_q --build-dir ./build_st <PATH_TO_THE_SAMPLE_CODE>
#to flash
west flash --build-dir ./build_st/
2025-11-17 11:04 PM
@Jocelyn RICARD any inputs on above question?
2025-11-24 9:22 AM
Hello @SAMINA ,
Sorry, I can't help you on Zephyr part. I'm not used to it and have not enough time to learn this.
You may log a ticket.
Best regards
Jocelyn
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.