2021-03-11 8:54 AM
I've been able to compile previous versions of SBSFU (P-NUCLEO-WB55.Nucleo/Applications/1_Image) without issues, but with this one I've run into two issues:
First, SE code did not fit in SE_ROM_region. I was able to fix this by adjusting the linker map and MPU region definitions.
Second, I get this error when compiling the UserApp project:
c:\st\stm32cubeide_1.1.0\stm32cubeide\plugins\com.st.stm32cube.ide.mcu.externaltools.gnu-tools-for-stm32.9-2020-q2-update.win32_1.5.0.202011040924\tools\arm-none-eabi\bin\ld.exe: ../../../../1_Image_SBSFU/SW4STM32/STM32WB55RG_Nucleo_1_Image_SBSFU/Debug\se_interface_app.o: in function `SE_APP_GetActiveFwInfo':
(.SE_IF_Code+0x0): multiple definition of `SE_APP_GetActiveFwInfo'; ../../../../1_Image_SBSFU/SW4STM32/STM32WB55RG_Nucleo_1_Image_SBSFU/Debug\se_interface_app.o:(.SE_IF_Code+0x0): first defined hereIf I search the SBSFU projects for "SE_APP_GetActiveFwInfo", I find the definition in se_interface_application.c (in the SBSFU project), the declaration in se_interface_application.c (also in the SBSFU project) and a single call in se_user_code.c (in the UserApp project). It's hard for me to see how there could be multiple definitions here. Any debugging advice would be greatly appreciated.
Thanks!
Solved! Go to Solution.
2021-03-11 9:40 AM
Hello,
this build issue is very probably the same described here:
This is related to latest release 1.6.0 of STM32CubeIDE. The solution is provide in this other post.
Best regards
Jocelyn
2021-03-11 9:40 AM
Hello,
this build issue is very probably the same described here:
This is related to latest release 1.6.0 of STM32CubeIDE. The solution is provide in this other post.
Best regards
Jocelyn
2021-03-11 10:29 AM
That did it. Thanks again!
2021-07-07 6:24 AM
Hi
I solved the problem by disconnecting and connecting the stm32-wl55c1 from my PC while pressing Debug botton in Cube-IDE.
Amin TAYEBI
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.