2025-01-24 4:18 AM - last edited on 2025-01-24 4:28 AM by Andrew Neil
Title edited to be more descriptive than just "USB"
HI,
I Need help, My application Requires Firmware updates using USB DFU Mode, and planning to make a custom Pc software that updates code using USB. How can I Make sure that only my Pc software should have access to connect the STM 32 using USB and update the code , How i can implement this security feature in My application? Does the USB library provide any authentication techniques So that I can integrate it for My custom application?
Thanks and Regards
JIJO
2025-01-24 1:10 PM
Newer STM32 chips (i.e. STM32N6) have more advanced and complicated security settings like this. I would suggest reading up on those and determining if those are sufficient. Also read up on SBSFU to see if that is acceptable.
In general, if someone wants to change the firmware on a chip, you are not going to be able to fully prevent it. Consider the case where the chip is physically replaced.
2025-02-04 8:59 PM
Hello,
SBSFU examples are there for Y modem Protocol for updates Is it Possible for USB DFU?
2025-02-04 10:00 PM
You may start with the How to use the ST Open Bootloader for STM32 Microc... - STMicroelectronics Community code and extend that to your needs.
There are 3rd party bootloaders like homepage [OpenBLT Bootloader] which has a dual (commercial/open source) licensing model. Here they are discussing security features: Security options of the OpenBLT bootloader - Feaser Developer Blog
hth
KnarfB
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.