2025-01-29 1:54 AM - edited 2025-01-29 1:57 AM
Hi,
I'm currently experimenting with the decryption of custom data provisioned into the OBKeys storage with hardware encryption enabled.
I've successfully provisioned the data without encryption and read it back intact. With encryption enabled, I see that the data that I read back is different after every new provisioning/code change attempt which is as I expect, but I have not successfully decrypted it. My code is based on code in low_level_obkeys.c from one of the Nucleo H533RE OEMiROT_Boot application examples. Here's my code with error checking removed for compactness (no errors are returned, the code runs fine, just the output is not correct). Note: temp_data contains the encrypted data exactly as read from the OBKeys region. Once I get this working, I guess I'll just try decrypt directly from the OBKeys region.
CRYP_HandleTypeDef hcryp = { 0U };
uint32_t a_aes_iv[4] = {0x8001D1CEU, 0xD1CED1CEU, 0xD1CE8001U, 0xCED1CED1U};
__HAL_RCC_SBS_CLK_ENABLE();
__HAL_RCC_SAES_CLK_ENABLE();
WRITE_REG(SBS_S->EPOCHSELCR, SBS_EPOCHSELCR_EPOCH_SEL_0);
hcryp.Instance = SAES_S;
HAL_CRYP_DeInit(&hcryp);
hcryp.Init.DataType = CRYP_NO_SWAP;
hcryp.Init.KeySelect = CRYP_KEYSEL_HW; /* Hardware unique key (256-bits) */
hcryp.Init.Algorithm = CRYP_AES_CBC;
hcryp.Init.KeyMode = CRYP_KEYMODE_NORMAL;
hcryp.Init.KeySize = CRYP_KEYSIZE_256B; /* 256 bits AES Key*/
hcryp.Init.pInitVect = a_aes_iv;
HAL_CRYP_Init(&hcryp);
HAL_CRYP_Decrypt(&hcryp, (uint32_t*)temp_data, (uint16_t)(sizeof(temp_data) / 4U), (uint32_t*)obkey_data, 100);
HAL_CRYP_DeInit(&hcryp);
I've tried different options for the Algorithm (ECB and CTR), I've tried DataType as BYTE_SWAP and I've tried leaving the InitVect as null (I don't know what the magic numbers in a_aes_iv represent, I suspect they are memory addresses and figure this could be the root of my problem.
My data is stored in OBKeys Level 1 at 0x0ffd0160, right after the DA certificate data. As mentioned before, I can read it back and see the same values as I get in the CubeProgrammer Device memory tab after debug authentication. My process for running the code is to write the application to the device when it is 'Open', activate TrustZone, change the Product State to Provisioning and accept the offer for the default DA certificate, provision my custom data, change the Product state to iRoT-provisioned. All performed using CubeProgrammer GUI.
What am I doing wrong here? How do I decrypt custom data using the HUK?
Best regards,
Michael Waites
Solved! Go to Solution.
2025-01-31 9:28 AM
2025-01-29 2:22 AM
Hello @MichaelWaites ,
could you please make sure that SAES device is allocated to secure ?
By default all peripherals are non secure.
Basically you should have something like:
__HAL_RCC_GTZC1_CLK_ENABLE();
HAL_GTZC_TZSC_ConfigPeriphAttributes(GTZC_PERIPH_SAES, GTZC_TZSC_PERIPH_SEC|GTZC_TZSC_PERIPH_PRIV);
Best regards
Jocelyn
2025-01-29 6:07 AM - edited 2025-01-30 4:55 AM
Hi @Jocelyn RICARD ,
I did not have those settings you suggested, so to try ensure all settings are correct, I've started a new project in CubeIDE with TrustZone enabled and configured the minimum settings that I believe I need to make the test work.
CubeIDE generated the ConfigPeriphAttributes calls (for SAES and RNG) but did not seem to generate a call for GTZC1_CLK_ENABLE, so I added that myself.
All my previously posted code and process are the same, but I still do not manage to decrypt the OBKey data correctly.
Does anything look wrong in the code I posted above, or my process?
Thanks,
Michael
2025-01-31 3:47 AM
Hi @Jocelyn RICARD,
Are you able to provide more help for this? With changes in made in your previous response, I am still unable to decrypt the custom data successfully with any of the encryption parameters I have tried.
Thanks,
Michael
2025-01-31 5:28 AM
Hello @MichaelWaites ,
Yes, I'm sorry, I need some time to try to reproduce your issue. I will come back to you asap
Best regards
Jocelyn
2025-01-31 9:28 AM
2025-02-03 2:51 AM
Thanks for the example. I was able to provision the device following my own procedure and to modify the source to decrypt and dump my custom data successfully.
I've not yet worked out what is different in your demo project compared to mine which is preventing mine from working, but I'll mark your answer as the solution and post additional info for the benefit of others when I work out where I've gone wrong.
Thanks for your time,
Michael
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.