2020-08-12 12:15 AM
Hi,
We are using SPSGRF-868 module in our project, With following settings of RF module operating @868 MHz Send/receive data without Encryption we are able to achieve 20~25 meter distance and working fine. But Send/Receive the data with encryption we are not able to achieve 20~25 meters distance.
We followed below settings for with/without encryption:
Date rate: 3.6 Ksps
Frequency deviation : 9.918 KHz
Channel filter : 50.961 KHz
is it as payload size increases range is degraded and is it need to be change above settings for Send/Receive data with encryption to achieve 20~ 25 meters distance?
Thanks,
Nagaraj
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.