2024-10-17 7:10 AM
Hi @Jocelyn RICARD,
My team developed Android app with following code to encrypt the message then send it to STM32WB55 device via BLE :
...
SecretKeySpec secretKeySpec = new SecretKeySpec(secretKey, "AES");
IvParameterSpec parameterSpec = new IvParameterSpec(iv);
Cipher cipher = Cipher.getInstance("AES/CCM/NoPadding");
cipher.init(Cipher.ENCRYPT_MODE, secretKeySpec, parameterSpec);
return cipher.doFinal(message);
This code has no tag/addData inputs.
First attempt:
I develop the following code to decrypt the encrypted message on STM32WB55 device with AddData/Tag variables filled 0 because I dont use them:
const uint8_t AddData[] =
{
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00,
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};
const uint8_t Expected_Tag[] =
{
0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00, 0x00
};
cretval = cmox_aead_decrypt(CMOX_AES_CCM_DEC_ALGO, /* Use AES CBC algorithm */
blePkocEncryptedData, encryptedDataLen, /* Ciphertext to decrypt */
sizeof(Expected_Tag),
blePkocSharedKeyData, sizeof(blePkocSharedKeyData), /* AES key to use */
IV, sizeof(IV), /* Initialization vector */
AddData, sizeof(AddData),
blePkocDecryptedData, &computed_size); /* Data buffer to receive generated plaintext */
After executed this cmox_aead_decrypt() function, I got the result = CMOX_CIPHER_AUTH_FAIL.
Second attempt:
I develop the following code on STM32WB55 device with NULL to AddData/Tag variables because I dont use them:
cretval = cmox_aead_decrypt(CMOX_AES_CCM_DEC_ALGO, /* Use AES CBC algorithm */
blePkocEncryptedData, encryptedDataLen, /* Ciphertext to decrypt */
0,
blePkocSharedKeyData, sizeof(blePkocSharedKeyData), /* AES key to use */
IV, sizeof(IV), /* Initialization vector */
NULL, 0,
blePkocDecryptedData, &computed_size); /* Data buffer to receive generated plaintext */
After executed this cmox_aead_decrypt() function, I got the result = CMOX_CIPHER_ERR_BAD_PARAMETER.
How to use this function without tag/addData inputs ?
Thanks
Gregory Saint-Jean
Solved! Go to Solution.
2024-10-28 6:27 AM
Hello @Jocelyn RICARD ,
I finally fixed this issue by adding the following code in Android app :
cipher.updateAAD(new byte[]{0x00});
Thank you
Gregory
2024-10-17 9:37 AM
Hello @GSain.1 ,
The TAG is normally added to the encrypted message
You should be able to find this information just by checking the size of the ciphered message on Android side.
I would guess tag size is 16.
The additional data is not mandatory so setting NULL pointer and size 0 is OK.
So, you should have an encrypted data that is "tagsize" bytes bigger than the message with the TAG at the end.
Providing the good tag size in your second attempt should work
Best regards
Jocelyn
2024-10-18 6:16 AM
Hello @Jocelyn RICARD ,
I tried to set tag size = 16 and addData = null without success because I always got CMOX_CIPHER_ERR_BAD_PARAMETER.
cretval = cmox_aead_decrypt(CMOX_AES_CCM_DEC_ALGO, /* Use AES CBC algorithm */
blePkocEncryptedData, encryptedDataLen, /* Ciphertext to decrypt */
//sizeof(Expected_Tag),
16,
blePkocSharedKeyData, sizeof(blePkocSharedKeyData), /* AES key to use */
IV, sizeof(IV), /* Initialization vector */
NULL, 0,
blePkocDecryptedData, &computed_size); /* Data buffer to receive generated plaintext */
Thanks
Gregory
2024-10-18 7:02 AM
Hello @GSain.1 ,
Well I could reproduce your issue. For some reason the function is not checking size before checking buffer.
So, please create a dummy buffer like uint8_t p[]={0}; and provide p instead of NULL for the add data pointer.
Best regards
Jocelyn
2024-10-28 6:27 AM
Hello @Jocelyn RICARD ,
I finally fixed this issue by adding the following code in Android app :
cipher.updateAAD(new byte[]{0x00});
Thank you
Gregory
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.