2023-03-08 2:57 AM
For storing my crypto key I'm using the following function to store the key in the WB55 core 2 secure key storage:
uint8_t key_index = 1;
SHCI_CmdStatus_t result;
SHCI_C2_FUS_StoreUsrKey_Cmd_Param_t CKS_param;
CKS_param.KeyType = KEYTYPE_SIMPLE;
CKS_param.KeySize = KEYSIZE_32;
memcpy(CKS_param.KeyData, key, KEYSIZE_32);
result = SHCI_C2_FUS_StoreUsrKey(&CKS_param, &key_index);
DPRINTF("Key stored at index: %d", key_index);And than loading it into the aes crypto peripheral.
Al works fine until the index reaches the end positions(100 keys).
After that writing a new key will always fail.
I can't find a function to wipe the user key(s).
I there a way to achieve this?
How can i wipe or overwrite a user key?
I think I misunderstand the use of CKS...
2024-04-12 3:12 AM
Hello @dd1 ,
Sorry for the delayed response. The maximum of keys that can be stored using FUS is 100 as stated in AN5185 (see section 5.1 Key types and structure) +one master clear key used to decrypt other keys if they are stored as encrypted. once stored you cannot neither remove nor update a key this is done to prevent key tampering as explained in this post.
BR
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.