STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Porting STM32CubeExpansion_Cloud_AWS to STM32H563ZI

Hello everyone, I hope you are well.I'm working on a project and one of the requirements is connection to AWS, so I chose to start with the STM32H573I-DK kit, where following the "STM32CubeExpansion_Cloud_AWS_H5_V1.0.0" step by step I managed to conn...

ffjunq by Associate III
  • 1894 Views
  • 2 replies
  • 0 kudos

Resolved! STM32CubeU5 TFM swap strategy, secure loader

Hello,I am working with STM32CubeU5 TFM v1.5 for STM32 u585. I develop a custom loader using CAN communication. First I used MCUBOOT_OVERWRITE_ONLY and MCUBOOT_PRIMARY_ONLY setup. The CAN communication worked fine (in non-secure loader).Then I switch...

ppedro by Associate II
  • 3489 Views
  • 5 replies
  • 0 kudos

STiROT_OEMuROT example results in hard fault

Dear community,I have been experimenting with secure boot on the STM32H573I-DK using the latest git checkout of STM32CubeH5 (see https://github.com/STMicroelectronics/STM32CubeH5).The STiROT and OEMiROT examples run fine out-of-the-box. However, when...

jens-vdb by Associate II
  • 4323 Views
  • 6 replies
  • 0 kudos

SBSFU on stm32g070rb

I'm interested in understanding the modifications required to adapt the 'STM32Trust security framework' code, accessible on the STM website for STM32L5, for my project of developing a secure bootloader code specifically designed for the STM32G070RB. ...

AM15 by Associate
  • 1366 Views
  • 2 replies
  • 0 kudos

Resolved! STM32WB FUS CKS, no option to delete or overwrite userkeys?

From AN5185 I understand that up to 100 keys can be send to FUS for storage, but any index will only be written once. So once I have reached 100 writes, e.g. because I have constant pairing keys between devices but I allow to disengage and reengage s...

OliM by Senior II
  • 2129 Views
  • 1 replies
  • 0 kudos

How to reset sbsfu or unlock my flash memory??

I'm porting my project(sbsfu Nucleo-h753zi to Nucleo-h745zi-q)and i checked protection my board, but i can't full chip erase../STM32_Programmer_CLI.exe -c port=swd mode=UR -ob PROT_AREA_START1=0xFF PROT_AREA_END1=0 RDP=0xAA---------------------------...

yolominwoo_0-1711588452173.png yolominwoo_0-1711605169771.png
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.