2026-01-28 12:05 PM
Hi
I have been testing secure function calls from non-secure world in STM32U575 - TrustZone Enabled environment.
I have a LED_Port which is in secure world (secure peripheral). I have implemented a toggle function in secure project - secure_nsc.c/h
CMSE_NS_ENTRY void SECURE_BlinkBlueLED(void) {...}
I can be able to compile without any issues:
Here are some linker details:
.....................................
I verified the map files as below
.......................
Now I am calling this function from non-secure project: It went to Hard Fault as it calls original function which is in the secure world.
How to call veneer instead of direct function?
Any help?
2026-01-29 1:37 AM
Hello @Suthan
On STM32U5 with TrustZone, the non‑secure code must never call the secure implementation directly; instead, it has to call the veneer located in the NSC (Non‑Secure Callable) region. To achieve this, the function must be declared with `CMSE_NS_ENTRY` in a source file that is linked into the NSC region (for example `secure_nsc.c`), and the non‑secure project must include the corresponding NSC header (for example `secure_nsc.h`) and call that symbol. Please verify that `secure_nsc.o` is placed in the NSC section in the secure linker script and that in your non‑secure map file the symbol `SECURE_BlinkBlueLED` points to an address in the NSC region; otherwise the non‑secure code will attempt to jump directly into secure flash and trigger a HardFault.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.