2023-11-07 6:13 PM
Hi,
I have been trying to use P-Nucleo-WB55 project from SBSFU 2.6.2 with SECBOOT_AES128_GCM_AES_128_GCM_AES128_GCM crypto option. I have disabled all security IPs for ease of debugging and have tried with local loader and no loader configurations. I am using STM32 IDE and following all steps. Infact the SECBOOT_ECCDSA_WITHOUT_ENCRYPT_SHA256 crypto option works for me under same settings.
However, I am never able to use this crypto option to successfully decrypt and execute UserApp.
Has anyone been able to use this crypto option with P-Nucleo-WB55 project.
Solved! Go to Solution.
2023-11-07 11:43 PM
Hi,
have you provisioned AES key ?
This is describe in the readme.txt in SECorebin.
For example:
STM32CubeExpansion_SBSFU_V2.6.2\Projects\P-NUCLEO-WB55.Nucleo\Applications\2_Images\2_Images_SECoreBin\readme.txt
"5. Provisioning AES key in index 0x1
- STM32_Programmer_CLI.exe -c port=usb1 -wusrkey OEM_KEY_COMPANY1_key_AES_CBC.bin keytype=1
- this step can be done only once. Index will be incremented at each command but our example requires key to be
located at index 0x1 (SBSFU_AES_KEY_IDX)."
2023-11-07 11:43 PM
Hi,
have you provisioned AES key ?
This is describe in the readme.txt in SECorebin.
For example:
STM32CubeExpansion_SBSFU_V2.6.2\Projects\P-NUCLEO-WB55.Nucleo\Applications\2_Images\2_Images_SECoreBin\readme.txt
"5. Provisioning AES key in index 0x1
- STM32_Programmer_CLI.exe -c port=usb1 -wusrkey OEM_KEY_COMPANY1_key_AES_CBC.bin keytype=1
- this step can be done only once. Index will be incremented at each command but our example requires key to be
located at index 0x1 (SBSFU_AES_KEY_IDX)."
2023-11-08 8:58 AM
Hi Frantz,
No, I didn't provision the AES key since my understanding is that we don't need to provision key for SECBOOT_AES128_GCM_AES_128_GCM_AES128_GCM crypto. I was under the impression that only AES-CBC requires key provisioning.
I am slightly confused if it is necessary to provision AES key for AES-GCM option since I was able to use the same configuration for L476RG project without provisioning AES key.
2023-11-17 11:43 AM
Update: It turned out that the issue was in provisioning key. I needed to provision key for AES-GCM too.
After provisioning key, I was able to use SBSFU as intended. It is interesting to see that my STM32 programmer or CLI do not return index of the key after writing AES key(as expected from the instructions in readme).
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.