2024-04-08 7:41 AM - edited 2024-04-08 7:56 AM
Hello,
I am working with STM32CubeU5 TFM v1.5 for STM32 u585. I develop a custom loader using CAN communication. First I used MCUBOOT_OVERWRITE_ONLY and MCUBOOT_PRIMARY_ONLY setup. The CAN communication worked fine (in non-secure loader).
Then I switched to swap strategy (MCUBOOT_OVERWRITE_ONLY and MCUBOOT_PRIMARY_ONLY not defined). The CAN communication stopped working. After quite some investigation I found out that the reason is that the FDCAN IRQ is not enabled (although set to be enabled). Then I found out that the reason is probably due to the FDCAN1_IT0_IRQn is not set in ITNS1 for the non-secure domain. This can be handled in the secure loader.
Unfortunately, in this mode the secure loader is not used. I am not sure why, did I misconfigure or misunderstand something?
Any advise how to get interrupt enabled in the the non-secure loader in this mode?
Thanx.
Best regards,
peter
Solved! Go to Solution.
2024-04-16 9:50 AM
Hello @ppedro ,
following OLS case you made, I shared with you a working project that re-enables the secure loader to be able to make necessary configuration for your loader and with non secure loader size increase.
I also created an internal case to get back this secure part of the loader whatever the configuration.
I hope this will fit your needs
Best regards
Jocelyn
2024-04-09 12:03 AM
Hello,
it is the postbuild.sh script (loader) that switches if to include the secure loader in the loader image. It is size of secure_nsclib.o that switches one or the other way.
I forced to skip this and got an error when flashing the loader.bin:
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
I see two ways to go:
- playing with loader (secure / non-secure) sizes to fit into limits
- making loader pure secure implementation
Please, let me know if I am mistaken in my observations and what ways out you see?
Thanx.
Best regards,
peter
2024-04-09 3:20 AM
Hello,
I tweaked with the ns loader size and managed to decrease it. I came to some limits that I cant decrease any more.
Looking at the UM2851, Memory layout for the swap mode, Figure 10 shows:
Non-secure local loader space available is 24 kB. Below that is Unused 112 kB. Is there a way to use this unused space and thus having 136 kB for the non-secure local loader?
Best regards,
peter
2024-04-10 12:10 AM
Hello again,
in order to summarize my problem and questions / help I need to resolve it is as follows:
Thus I need to answer the following:
Or please correct me if my observations / findings / understandings are wrong.
Any help / advise is highly appreciated.
Thanx.
Best regards,
peter
2024-04-16 9:50 AM
Hello @ppedro ,
following OLS case you made, I shared with you a working project that re-enables the secure loader to be able to make necessary configuration for your loader and with non secure loader size increase.
I also created an internal case to get back this secure part of the loader whatever the configuration.
I hope this will fit your needs
Best regards
Jocelyn
2024-04-17 5:15 AM
Hello Jocelyn,
thanx for the solution you made in OLS case. It's working as expected.
Thanx.
Best regards,
peter
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.