2024-07-26 1:00 AM
I want to use SBSFU for a SW Update OTA Project , i try to compile the example project from SBSFU-Projects:
NUCLEO-G474RE_2_Images_SBSFU
NUCLEO-G474RE_2_Images_SECoreBin (first, this project will be compile)
NUCLEO-G474RE_2_Images_UserApp
by try to compile the "NUCLEO-G474RE_2_Images_SECoreBin Project", i get following error:
09:36:29 **** Build of configuration Debug for project NUCLEO-G474RE_2_Images_SECoreBin ****
make all
"../prebuild.sh" "../"
prepareimage with python script
python /prepareimage.py conf ..//../Inc/se_crypto_config.h
python: can't open file 'C:\\prepareimage.py': [Errno 2] No such file or directory
selected
../prebuild.sh: line 55: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 56: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 57: can't create ..//Application/Startup/se_key.s: nonexistent directory
../prebuild.sh: line 136: can't create ..//Application/Startup/se_key.s: nonexistent directory
recopy postbuild.sh script with .sh script
cat: can't open '..//.sh': No such file or directory
cat ..//.sh : failed
make[1]: *** [makefile:94: pre-build] Error 1
make: *** [makefile:62: all] Error 2
"make all" terminated with exit code 2. Build might be incomplete.
09:36:30 Build Failed. 2 errors, 0 warnings. (took 938ms)
I checked, that the "win folder" for prepareimage executable is there
can you please support with this topic?
Thanks
2024-07-26 1:40 AM
Hello @rojedagRH ,
you seem to have an issue with your version of STM32CubeIDE.
I remember one version, something like 6 months ago had a regression in the busybox where 'pwd' command didn't work. I think this was version 1.14.0 and was rapidly fixed with 1.14.1
So, if you update your STM32CubeIDE to more recent version it will solve your issue
Best regards
Jocelyn
2024-07-26 4:18 AM
Thanks, i updated the STM32CubeIDE from 1.14.0 to 1.16.0 and the "compile" is working!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.