STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Secure H743 firnware programming GUI tools

I've read the X-CUBE-SBSFU Secure Boot and Secure Firmware documents and it doesn't explain if these are tools, with GUI, or just an API, which should really be explained at the start.If you know all about it I am sure these documents are just great,...

Robmar by Senior III
  • 2615 Views
  • 4 replies
  • 2 kudos

Resolved! SBSFU-UserApplication-Debugging

I'm curious what is the best way to debug a User Application when using SBSFU on a STM32.Of course the security mechanisms in SBSFU/SECore must be disabled to allow debugging at all and basically just downloading the UserApplication and debug it with...

STM32H725 - RDP locked to BB

Hello, I have a problem with a STM32H725, the Option byte RDP is locked to the value BB.In fact, I try to change other option bytes and it always fail with this error: " Error: Option Byte Programming failed Or modified by application after OB_LAUNCH...

Dams by Associate III
  • 2357 Views
  • 3 replies
  • 0 kudos

Asymmetric Cryptography in STM

Hello,I’m working on a project using the STM32WLxx MCU and need guidance on implementing asymmetric cryptography (encryption, decryption, and key management). The MCU supports AES for symmetric encryption, but I’m looking for a solution for asymmetri...

Anubrata by Associate
  • 1517 Views
  • 1 replies
  • 2 kudos

Resolved! SBSFU STM32l476

Hi,I am working on SBSFU with stm32L476 Nucleo Board I am following the steps of Tutorial Security Part6 - STM32 security ecosystem - 02 Building the SBSFUI have Download Stm32CubeExpansion_SBFU_V2.6 but which is the highlighted directory are missing...

Prakash_Raj1994_1-1734591463772.png

Resolved! is RDP LEVEL 1  Enough?

hiplease only ST Employee answer this questioni use  this code for enable RDP LEVEL 1  for STM32H743 and STM32F407Can this code alone protect the program in the flash from any type of attack to read the program in the microcontroller?Will it be possi...

Natali by Associate III
  • 2575 Views
  • 3 replies
  • 3 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.