STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Unable to flash OEMiRoT application using STLink-V2

Hi,I'm developing a secure boot application for STM32H563ZI microcontroller. I started with a very simple application following ST template code and tutorials like this one: https://wiki.st.com/stm32mcu/wiki/Security:How_to_start_with_STM32CubeMX_OEM...

Can't enable PCROP on STM32H7

I try to enable the PCROP Feature on a STM32H753I am using the STM32CubeProgrammer and connect via ST-Link V2After connecting, I go to the "OB" page and set the PROT_AREA_END1 value to 0xFFF and activate the DMEP1Then I press the "Apply" button and t...

Moritz1 by Associate III
  • 363 Views
  • 2 replies
  • 1 kudos

Resolved! STM32H563 OEMiROT Non-Secure Application flash size

Hello,starting from the example application of the OEMiRot boot project, I noticed that the NS application size is limited to 640kB in the flash_layout.h  (#define FLASH_NS_PARTITION_SIZE (0xA0000) /* 640 KB for NS partition */)Since there is 1MB ava...

Resolved! STM32U5A5 Trustzone Application

Hi!I'm working on a Trustzone enabled application in STM32U5A5 nucleo board and have some questions in my mind. I have used the configurations of the example project for the Trustzone, which you can find below: - TZEN=1 - SECWM1_PSTRT=0x0 SECWM1_PE...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.