STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Confusion about rebuilding projects

I am using STM32CubeIDE and am slightly confused on the rebuilding project steps of the UM2262 manual. Should I be going into each individual folder in the "Projects" folder and rebuilding all of them (such as NUCLEO76RG --> Applications --> 2_Images...

APara.5 by Associate II
  • 1135 Views
  • 1 replies
  • 0 kudos

Resolved! How can i reset the HDP2EN to 0

Currently, i working on the nucleo-L552zeq and i run the SBSFU exemple propose by the cubeL5. i use the script regression.sh and the script the SBSFU_UPDATE.sh to initialize the board and download the firmware. this example can work normally on the b...

0693W00000Ba1ADQAZ.png 0693W00000Ba1AwQAJ.png 0693W00000Ba1BkQAJ.png
HQIN.1 by Associate
  • 1301 Views
  • 1 replies
  • 0 kudos

stm32L152RE sbsfu does not jump to user application code

I have updated the startup scripts from the MOOC to work with the stm32l152re. However, when I build the user app and flash it onto the MCU I only get the text from the SBSFU in the terminal. It automatically wants to receive a new user firmware:= [S...

Resolved! how to create own private key in sbsfu

Hi all, I am trying to make an own private key on the SBSFU, if anyone has succeeded in this could you pass me the steps which I have to proceed with. I went through An5056, then I tried to change ECCkey1 but in some cases. it works and it is upgradi...

Roshan by Associate III
  • 1814 Views
  • 1 replies
  • 0 kudos

Resolved! H753ZI board unaccessible after download of incomplete secure boot

Hello,I want to integrate a secure boot and secure software update (SBSFU) on a nucleo H753ZI board.I downloaded the software from https://www.st.com/en/embedded-software/x-cube-sbsfu.html and followed the steps to compile the three programs (SECore,...

0693W00000APJdCQAX.png 0693W00000APJd7QAH.png
EBonv by Associate III
  • 7499 Views
  • 13 replies
  • 0 kudos

Installation not validated:

I have implemented sbsfu on my board. It is running. If I download a new firmware out of my user-app the new firmware is loaded, the flash is swaped and the new firmware starts up.If I reset the board, the bootloader says - Installation not validated...

peterd by Associate II
  • 1501 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.