post build path
need to add CRC to my binary. i.e. srec_catCan I add path to IDE to look for srec_cat, alternative what path are searched
Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.
need to add CRC to my binary. i.e. srec_catCan I add path to IDE to look for srec_cat, alternative what path are searched
I had a problem while uploading firmware into my custom board.I used ST-Link attached at NUCLEO-F091RC board, and I could read Option Bytes and Memory at 0x00000000 using ST-Link Utility and STM32CubeProgrammer.But I can't read or erase flash memo...
cant find and examples on how to use GenerateSignature
Hello,I need help setting the secure memory area for the STM32H753XI mcu. I am running it on STM32H753I-EVAL kit.I have read the dedicated part on the reference manual (chapter 5 on document RM0433), the "Introduction to STM32 microcontrollers securi...
hi there I cannot figure out the true meaning of htcr reg and config1~config3 field in rng_cr reg。 I was wondering about the relationship between health test register and health test parameter (repetition counter test the “40�? consecutive bi...
Hello,I have an unexpected behavior with a H753ZI board. After a very few steps, I ended up in a situation where PCROP seems to be enabled and RDP level is set to 0. For some reasons, this causes the board to freeze indefinitely, moreover after disco...
This may be a dumb question, but how can I correctly reboot a programmed board after setting the read out protection?Hardware: ST Link-V2Software : STM32 ST-LINK CLI v3.5.0.0Connect via SWD freq 4000Test programs BOR_LEV=3 and nDBANK=0 > everything i...
In the video, "Security Part6 - STM32 security ecosystem - 02 Building the SBSFU" there are some scripts under the folder "STM32SecuWS" which are unavailable in the SBSFU download software. Where can I get these scripts? I am also struggling while fo...
Hi,I followed document "readme.txt" in "STM32Cube_FW_L5_V1.4.0\Projects\STM32L562E-DK\Applications\TFM" to family with TFM, it work fine.My question:1: "press reset button or restart the board power" will lock the board. Please tell me what code in...
Using a STM32F407VGT6 (1MB Flash)For the starting address of 0x08000000 (base address), HAL_CRC_Accumulate only accepts a buffer length of up to 0x40000.For 0x080F0000, only buffer length up to 0x4000.For 0x080FF000, only buffer length up to 0x400.Fo...
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.