STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Huge user application binary file

Hello everyoneSo I've managed to build MY user app, where a lot of things programmed alongside sbsfu support.But the binary file is simply huge - 134 MB! How comes?Also, sfb file does not get generated. May it be connected to disabled security define...

leeana by Associate III
  • 1430 Views
  • 1 replies
  • 0 kudos

Resolved! STM32L496 header missing Hash peripheral definitions

It looks like STM32L496xx.h does not have the hash peripheral definitions in it. e.g. The STM32Cube_FW_L4_V1.16.0 examples for STM32L496 HASH peripheral are all configured to use the STM32L4A6xx. Does ST have a plan to update STM32L496xx.h?, or Is...

jrgert by Associate III
  • 2096 Views
  • 3 replies
  • 0 kudos

Terminal Connection to COM port for STM Security MOOC part 4

Hi, I'm in the process of going through the labs in part 4 of the ST Security MOOCs, specifically the hands on over here .https://www.youtube.com/watch?v=0CVplWZ8zls&list=PLnMKNibPkDnF0wt-ZI74SflnsBV4yKzkO&index=3The hands on asks to connect a termin...

0693W00000FCHbNQAX.jpg 0693W00000FCHbhQAH.jpg 0693W00000FCHZhQAP.jpg
RKher.1 by Associate III
  • 1073 Views
  • 1 replies
  • 1 kudos

Resolved! Undefined reference to __ICFEDIT_SE_Key_region_ROM_start__

I am trying to merge UserApp example into my existing project. Everything goes fine, except for the error mentioned in the title. I've checked that include list is identical to UserApp example, as well as Linker->Miscellaneous->Other flags. What am I...

leeana by Associate III
  • 2450 Views
  • 4 replies
  • 0 kudos

FreeRTOS with SBSFU is not working

I am using the STM32L562E-DK development kit. I have taken reference to NUCLEO-L552ZE-Q and ported it for STM32L562E-DK. Also added External OSPI flash. without FreeRTOS it is working fine.I have added FreeRTOS in the nonsecure application. For that,...

PYada.1 by Associate III
  • 8424 Views
  • 24 replies
  • 0 kudos

Resolved! How to call SecureEngine functions from my application?

Hello guys!How are u all?I'm having few issues to develop self-test on my application. I setup everything from the SBSFU side to check image handling flags, and its working fine. I'm able to set my new firmware to self-test state and check the state ...

MBuen.1 by Senior
  • 2732 Views
  • 5 replies
  • 0 kudos

STM32L562QEI6 enter Boot through USART interface

Hello,I have a system with one STM32L562QEI6 and one STM32F405RGT6, that is the main MCU.They communicate with USART interface.In the main CPU, boot0 and boot1 pins are phisically connected to VCC or GND through some resistors, so I can enter boot mo...

MFail.11 by Associate III
  • 3595 Views
  • 7 replies
  • 0 kudos

STM32L433RC SBSFU "Fw header authentication error"

Hello,I am trying to run the Secure boot feature on STM32L433RC using the SBSFU library example project (single image slot). The example project I am modifying is STM32L432KC board. Below are the modification/steps I made to example project to run on...

0693W00000FBO1KQAX.png
HDevi.1 by Associate II
  • 2569 Views
  • 2 replies
  • 1 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.