STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! TRNG in STM32L4R9I - EVAL pass ALL NIST Test ?

Hello !STM32L4R9I support True Random Number ( 32 bits per 1 time generation)I run an example and then make an program to generate 100.000.000 bits1 st iteration (100M bit) : HW is 0.5 and Passed NIST Test2 nd iteration (100M bit) : HW is 0.5001 and ...

TSang.3 by Associate
  • 3518 Views
  • 1 replies
  • 0 kudos

BLE ER key and IR key

I see that those keys are hardcoded in the code. As I understand they are responsible to LTK and CSRK.Should I change ERK and IRK between devices , so they are not the same? Asking for security reasons.

DS.4 by Senior II
  • 1317 Views
  • 1 replies
  • 0 kudos

Resolved! Issue with CRC32 module on STM32G483

Hi,I'm computing CRC32 with 04C11DB7 polynomial with different methods : through python binascii.crc32(...), on the following website " https://simplycalc.com/crc32-text.php ", and with ST embedded module on STM32G483.On basic strings such as "012345...

EPHIL.1 by Associate II
  • 4940 Views
  • 3 replies
  • 0 kudos

Resolved! problem with adding SMT32CubeExpansion_Crypto_V4.0.1

Hello,I am having some issues with adding SMT32CubeExpansion_Crypto_V4.0.1 to my stmcube environment. I am using stm cube 6.4. I go to Software Packs > Manage Software Packs > From Local... and then I point to SMT32CubeExpansion_Crypto_V4.0.1.zip, w...

VKnou.1 by Associate
  • 2148 Views
  • 1 replies
  • 1 kudos

Using Tamper with TF-M in STM32U5

Hi,In TFM and SBSFU applications, by default the anti-tamper protection is enabled for both internal tamper events and external tamper events. It is activated at the start of TFM_SBSFU_Boot, and remains active. In case of tamper detection, sensitive ...

ZKRAC.1 by Associate II
  • 7288 Views
  • 11 replies
  • 0 kudos

KMS Middleware supported STM32

What are the STM32 MCUs, support KMS middleware feature ??is STM32H753VI supported this KMS feature ??If NO, is there any way STM32H7 can generate Pair of Keys on the fly during run time to create Self Device Certificate ??

SPati.7 by Associate III
  • 1971 Views
  • 3 replies
  • 0 kudos

Not able to jump to application after enabling HDP

@JHOUD​ @TDK​ @Dimitrios Bako​ I have configured HDP as follows :By Bootloader .icf details are :define symbol __ICFEDIT_region_ROM_start__       = 0x0C000800;define symbol __ICFEDIT_region_ROM_end__        = 0x0C007FFF; Configurations when i debug t...

0693W00000LzCUYQA3.png 0693W00000LzCVgQAN.png
vsing.1 by Associate II
  • 2559 Views
  • 4 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.