STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! B-U585I-IOT02A TFM Application in STM32CubeIDE?

Hello,is there any example of a TFM application that is supported by STM32CubeIDE?I came across the iot-reference-stm32u5, but the structure of the project is way different from any other TrustZone and TFM examples available as part of the STM32CubeU...

amos3 by Associate III
  • 2130 Views
  • 2 replies
  • 0 kudos

AES encryption not working

Dear Team,I want use inbuild AES encryption engine to encrypt the data, therefore I used CubeMX to initialize the AES engine, when i'm going to encrypt the payload, it stuck in static HAL_StatusTypeDef CRYP_WaitOnOFNEFlag(CRYP_HandleTypeDef *hcryp,...

vchau.2 by Associate III
  • 3075 Views
  • 5 replies
  • 0 kudos

Hello, I am trying to implement the HKDF algorithm to generate a secret key, and I found a link containing an example of HKDF implementation ( you will find link below in details) but unfortunately, the code is incomplete and I have a few questions.

the link : https://wiki.st.com/stm32mcu/index.php?title=Security:How_to_implement_HKDF_with_the_Cryptographic_library&oldid=11796&diff=prev#HKDF_implementation_example_using_HMAC-SHA256_Cryptographic_library_services .my questions is first, once I ad...

WYous.1 by Associate III
  • 1276 Views
  • 0 replies
  • 1 kudos

STM32U5 Debug in RDP 0.5 With STM32CubeProgrammer

Hello,I am trying to start a debug session with STM32CubeIDE v1.11.2 on my board locked on RDP 0.5.I loaded a valid secure firmware which jumps into the non-secure firmware before setting RDP 0.5.I could connect STM32CubeProgrammmer and flash the non...

OOUES.1 by Associate
  • 3190 Views
  • 3 replies
  • 0 kudos

SB and SFU

Hey guys, I want to perform a firmware upgrade over the air. And use a UART to connect to IoT device.I use stm32l431xx and it contains hardware for symmetric encryption. And the host device which sends the binary uses stm32l496 has SBSFU.So I have a ...

Vmere.1 by Senior
  • 1298 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.