2024-08-02 8:43 AM - edited 2024-08-05 3:50 AM
Hello,
Unless I'm wrong, the architecture of the TFM application as described in UM2851 seems not to allow the assignment of a peripheral (e.g. a LED pin) to the Secure context of TrustZone as it is the case with simple TrustZone applications.
The UM2851 states that the user can "Replace the nonsecure TFM application example delivered in the STM32CubeU5 MCU Package by its own product nonsecure application", without raising this possibility for the secure application too.
Moreover, I couldn't find on the Internet such example of customization of the Secure context of the TFM application to assign peripherals to the Secure part of the application.
Is there a way to do so? If yes, how?
Thanks a lot.
@STea @Jocelyn RICARD @Benjamin BARATTE
Solved! Go to Solution.
2024-08-05 6:09 AM
Hello @SedCore ,
The previous reply was deleted because it was detected as AI generated spam.
know regarding your request, there is no restriction in changing the TFM Appli secure project in which you could assign change I/O attributions to the secure or non-secure world (check the target_cfg.c in secure Appli project).
I think by default it is configured for the non-secure world for SRAM3, so you need to modify the SAU and GTZC to be assigned to secure.
Regards
2024-08-05 3:21 AM
@gpguy :thinking_face: it seems you had some ideas? Why your reply has been deleted?
2024-08-05 6:09 AM
Hello @SedCore ,
The previous reply was deleted because it was detected as AI generated spam.
know regarding your request, there is no restriction in changing the TFM Appli secure project in which you could assign change I/O attributions to the secure or non-secure world (check the target_cfg.c in secure Appli project).
I think by default it is configured for the non-secure world for SRAM3, so you need to modify the SAU and GTZC to be assigned to secure.
Regards
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.