2020-05-06 8:57 AM
I'm trying to initialize windowed watchdog and get to work done in STM32F4 discovery board. I've a couple of doubts,
Below is my code:
/**
******************************************************************************
* @file main.c
* @author Ac6
* @version V1.0
* @date 01-December-2013
* @brief Default main function.
******************************************************************************
*/
/**********************************************************/
#include "stm32f4xx.h"
#include "stm32f4_discovery.h"
#include "stm32f4xx_hal.h"
#include "stdio.h"
extern void initialise_monitor_handles();
WWDG_HandleTypeDef hWWDG;
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_WWDG_Init(void);
int main(void)
{
// For printf we need to call this initialize function
initialise_monitor_handles();
HAL_Init();
SystemClock_Config();
MX_GPIO_Init();
MX_WWDG_Init();
// If watchdog is running then led will turn on
if(__HAL_RCC_GET_FLAG(RCC_FLAG_WWDGRST) == SET)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_SET);
__HAL_RCC_CLEAR_RESET_FLAGS();
}
else
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
}
while (1)
{
/* USER CODE END WHILE */
/* USER CODE BEGIN 3 */
if(HAL_GPIO_ReadPin(GPIOA,GPIO_PIN_0))
{
while(1);
}
// HAL_WWDG_Refresh(&hWWDG);
HAL_GPIO_TogglePin(GPIOD, GPIO_PIN_12);
HAL_Delay(1000);
HAL_WWDG_Refresh(&hWWDG);
}
}
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
uint32_t PCLK1_fre = 0;
__PWR_CLK_ENABLE();
__HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE2);
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
RCC_OscInitStruct.HSIState = RCC_HSI_ON;
RCC_OscInitStruct.HSICalibrationValue = 16;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
RCC_OscInitStruct.PLL.PLLM = 16;
RCC_OscInitStruct.PLL.PLLN = 336;
RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV4;
RCC_OscInitStruct.PLL.PLLQ = 7;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK | RCC_CLOCKTYPE_PCLK1 |RCC_CLOCKTYPE_PCLK2 | RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV2;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_2);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
HAL_NVIC_SetPriority(SysTick_IRQn,0,0);
PCLK1_fre = HAL_RCC_GetPCLK1Freq();
printf("PCLK frequency is: ");
printf(PCLK1_fre);
}
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct,GPIO_ButtonStruct;
__GPIOD_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_12, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_13, GPIO_PIN_RESET);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
GPIO_InitStruct.Pin = GPIO_PIN_12;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Pull = GPIO_NOPULL;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
// used pin 13 for watchdog clocked indication
GPIO_InitStruct.Pin = GPIO_PIN_13;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
// for watchdog initialization confirmation
GPIO_InitStruct.Pin = GPIO_PIN_15;
HAL_GPIO_Init(GPIOD, &GPIO_InitStruct);
GPIO_ButtonStruct.Pin = GPIO_PIN_0;
GPIO_ButtonStruct.Mode = GPIO_MODE_IT_RISING;
GPIO_ButtonStruct.Pull = GPIO_NOPULL;
GPIO_ButtonStruct.Speed = GPIO_SPEED_LOW;
GPIO_ButtonStruct.Pin = GPIO_PIN_0;
HAL_GPIO_Init(GPIOA,&GPIO_ButtonStruct);
}
static void MX_WWDG_Init(void)
{
WWDG_InitTypeDef WWDG_InitStruct;
// HAL_StatusTypeDef catchvariable;
hWWDG.Instance = WWDG;
// hWWDG.Init = WWDG_InitStruct;
WWDG_InitStruct.Prescaler = WWDG_PRESCALER_8;
WWDG_InitStruct.Window = 95;
WWDG_InitStruct.Counter = 127;
WWDG_InitStruct.EWIMode = WWDG_EWI_ENABLE;
if(HAL_WWDG_Init(&hWWDG) == HAL_OK)
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
HAL_Delay(2000);
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_RESET);
}else
{
HAL_GPIO_WritePin(GPIOD, GPIO_PIN_15, GPIO_PIN_SET);
}
}
/**********************************************************/
When I tried to debug using watchpoints i found, inside SystemClock_Config() function after __PWR_CLK_ENABLE() it redirected to startup_stm32f407xx.s and there is a inifinte loop code where it get trapped.
Below is the exact code:
/*************************************************************************/
/**
* @brief This is the code that gets called when the processor receives an
* unexpected interrupt. This simply enters an infinite loop, preserving
* the system state for examination by a debugger.
* @param None
* @retval None
*/
.section .text.Default_Handler,"ax",%progbits
Default_Handler:
Infinite_Loop:
b Infinite_Loop
.size Default_Handler, .-Default_Handler
/*************************************************************************/
2020-05-06 9:24 AM
PCLK1_fre = HAL_RCC_GetPCLK1Freq();
printf("PCLK frequency is: ");
printf(PCLK1_fre);That last printf statement won't work. PCLK1_fre is not a string.
Look at the SCB register to figure out which interrupt is active. VECTACTIVE bits.
2020-05-06 10:12 AM
Thanks for answer. It's going to infinite loop because of that printf statement, I resolve it by including "%d" in printf statement. But my watchdog is not getting reset. Can u suggest me where I'm doing wrong.
2020-05-06 11:34 AM
> But my watchdog is not getting reset.
Looks like your main loop calls HAL_WWDG_Refresh repeatedly. Why would the chip reset?
> GPIO_ButtonStruct.Mode = GPIO_MODE_IT_RISING;
Why not GPIO_MODE_INPUT?
2020-05-07 11:32 AM
I check with input mode also
GPIO_ButtonStruct.Mode = GPIO_MODE_INPUTBut it didn't work.
I used switch so that I can redirect cpu into an infinite loop and it worked but system is not getting reset. I tried with increasing time delay but that also not worked means system is not getting reset. I think there is problem in windowed watchdog initialization. Can u help me out where I'm making mistake?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.