2013-08-14 8:55 PM
Hello:
Today , I want to capture the high-level length of input signal using TIM5 Channel 1 (PA.0) in chip (STM32F103ZET6)?but why program can not enter TIM5 interrupt service ? please help me ! I have attached the project here #stm32f103zet6-tim52013-08-14 11:06 PM
Doesn't look unreasonable, I'd probably not be clearing interrupts immediately prior to exiting the service routine.
How are you testing the failure condition, are you breakpointing the TIM5_IRQHandler() ?2013-08-17 3:51 AM
Make sure that you are using startup_stmf10x_xl.s Standard lib..
2013-08-17 1:42 PM
Make sure that you are using startup_stmf10x_xl.s Standard lib..
How would that help? He has an HD part, not an XL one. And has a TIM5_IRQHandler in the vector table.2013-08-26 3:43 AM
Yes startup_stm32f10x_hd.s lib needed. I faced the same problem while im doing Capturing using the same board. By default it will add the (startup_stm32f10x_md.s) lib. In startup_stm32f10x_md.s lib there is no TIM5, so startup_stm32f10x_hd.s file has to be added..
2013-08-26 9:57 AM
I faced the same problem while im doing Capturing using the same board.
What board is that? The OP doesn't identify one, and it's not the STM32 VL-Discovery board. He also attaches a project that contains the right source files, and right defines for the HD part. From the project one might infer he has a Core103Z.By default it will add the (startup_stm32f10x_md.s) lib. What does? The template project, for the STM3210E-EVAL doesn't, or the VL-DISCOVERY. I can see that using the wrong file, with a vector table lacking the interrupt required, will be a problem. I'm just not seeing that in the project presented here. There is some other issue at play here. The OP has not responded.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.