2019-11-17 10:35 AM
The STM32H7 reference manual revision 6 gives the FastSinc response as:
However this seems to make no sense. The first part is a normal sinc^2 filter, but the second part describes an impulse + delayed impulse, which results in a quite strange frequency response.
I might expect the second part to be (1 - z^-(2*FOSR))/(1-z^-1) instead, but could there be two typos there? Then the first null in frequency response would be at Fs/(2 * FOSR), which would be quite useful.
If the response function described in manual is correct, it would be interesting to hear in what cases this FastSinc mode is useful?
2019-11-29 10:06 PM
Ok, now that I have the hardware I've tested the impulse response myself using this code:
static void cmd_dfsdm_test(BaseSequentialStream *chp, int argc, char *argv[])
{
RCC->APB2ENR |= RCC_APB2ENR_DFSDM1EN;
DFSDM1_Channel0->CHCFGR1 = DFSDM_CHCFGR1_DFSDMEN | DFSDM_CHCFGR1_DATMPX_1 | DFSDM_CHCFGR1_CHEN;
DFSDM1_Channel0->CHCFGR2 = 0;
DFSDM1_Filter0->FLTCR1 = DFSDM_FLTCR1_FAST | DFSDM_FLTCR1_RCONT;
DFSDM1_Filter0->FLTCR2 = 0;
DFSDM1_Filter0->FLTFCR = (0 << DFSDM_FLTFCR_FORD_Pos) | (2 << DFSDM_FLTFCR_FOSR_Pos) | (0 << DFSDM_FLTFCR_IOSR_Pos);
DFSDM1_Filter0->FLTCR1 |= DFSDM_FLTCR1_DFEN;
DFSDM1_Filter0->FLTCR1 |= DFSDM_FLTCR1_RSWSTART;
for (int i = 0; i < 1000; i++)
{
DFSDM1_Channel0->CHDATINR = (i == 100) ? 1 : 0;
if (DFSDM1_Filter0->FLTISR & DFSDM_FLTISR_REOCF)
{
chprintf(chp, "%8d %8d\n", i, DFSDM1_Filter0->FLTRDATAR >> 8);
}
}
}And found out the impulse response at FOSR=3 to be (0,3,0,3,0).
So the reference manual is correct.
I'd still be interested in know for what purpose this response is desirable, but at least I now know it is not suitable for my use case.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.