2026-02-02 11:34 AM - last edited on 2026-02-02 11:56 AM by Andrew Neil
Hi,
we are trying to get SDMMC1 running on our evaluation boards (STM32H757-EVAL) but without any success so far.
To further investigate the issue we started a new project from scratch, using CubeMX with sdmmc1 enabled. It doesn't work neither.
btw: board and SD interface are OK. i.e.the demo that came with the board is reading video files from SD card successfully.
Please, can someone provide a ruuning setup for Cube-MX (STM32H7 firmware 11 or 12) with the specific settings for Clock Configuration and SDMMC1.
We are using CubeMX 1.15, STM32H7 firmware package V. 12.1.
The error happens during SD PowerOn(), i.e. there is no response from CMD8, CMD55...
Thanks for your help
Tom
Solved! Go to Solution.
2026-02-03 6:23 AM
Thanks for the hint.
I also checked the examples for the STM32H747-EVAL, specifically the JPEG example that reads an image from SD card. That project was buildiung and running without any problems AND :) after switching to our own Project it was running, i.e SDMMC initialization ok...
BUT just once :( After reset or board power cycle we see the same error as before, i.e. as in my original post.
It seems to me that in our project the SD card is left in some strange/undefined state if the evaluation board is powered down.
We'll furthre investigate this behaviour.
2026-02-03 12:24 AM
Hello @TomHoMe and welcome to the ST community,
You may need to inspire from the BSP driver especially the file https://github.com/STMicroelectronics/stm32h747i-eval-bsp/blob/7d2997a570932f0b2f30be33209e94d3423226f4/stm32h747i_eval_sd.c unfortunately there is no ioc file. You need to reflect that config into your CubeMx configuration.
2026-02-03 6:23 AM
Thanks for the hint.
I also checked the examples for the STM32H747-EVAL, specifically the JPEG example that reads an image from SD card. That project was buildiung and running without any problems AND :) after switching to our own Project it was running, i.e SDMMC initialization ok...
BUT just once :( After reset or board power cycle we see the same error as before, i.e. as in my original post.
It seems to me that in our project the SD card is left in some strange/undefined state if the evaluation board is powered down.
We'll furthre investigate this behaviour.
2026-02-24 7:35 AM
Hi,
I'm back from vacation and wanted to briefly share the solution.
The example code, mentioned obove, showed me that the tranceiver voltage control (3.3V -> 1.8V) and the detect signal only work via the MFX interface (I/O expander).
Hence, I configured the SDMCC peripherals using CubeMX and disabled code generation for MX_SDMMC1_SD_init in the project settings. Instead of generated MX_SDMMC1_SD_init, I'm using the initialization code from the example project, i.e., calling BSP_SD_Init.
Now everything works as expected.
Regards,
Tom
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.