2018-10-12 10:20 AM
I've accidentally unplugged USB cable during debugging. I can still upload new programs, and they seem to work just fine, but the RGBled LD1 is constant orange/red(i cant tell) and should be green after successful download... and i can't erase chip with STlinkUtility tool, or with Demonstrator GUI tool.
In STlinkUtility tool i can connect the board, but when I try to do a 'full chip erase', i get message saying : " The elf loader Sector Erase function fails.: Error occured during flash mass erase! "
I may not remember correctly but i think that after downloading new program on a board the LD1 should be green. The board is still functional, but I just don't want to work with faulty board, if it is. Hope you could help me.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.