STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to make I2C work?

Hi ,I'm currently working on a STM32F103C8T6 and i need to use the I2C port.I use the STM32 cube MX software to create the project. (like that all my ports are set).I use STM32 System Worckbench to code.My problem is that i don't achieve to communica...

DSimo.19 by Associate
  • 1397 Views
  • 1 replies
  • 0 kudos

STM32L1 and low power stop mode

Posted on March 28, 2017 at 12:26Hi,I am using a https://community.st.com/tags♯/?tags=stm32l1 on the STM32L152c-discovery and trying to reach a lower power consumption.But I can't reach less than 0.6mA !!! (10x more than in theory).Where this curren...

samuel23 by Associate III
  • 1976 Views
  • 3 replies
  • 0 kudos

STM32H743/753/750 RM0433 Rev 5 documentation feedback

Section 37.4.3: TS[4:0] - setting 00010 is missing definitionSame section, Table​ 322, section 38.4.3 Table 327, section 39.4.3 Table 330, section 40.5.3 Table 335 all show the same type of information but are completely different formats. IMO, Table...

Resolved! Replacement of STM32F334R8T7 with Low Power MCU

I am Looking for Low power MCU in LQPF64 Package. I found too many MCU , those could be compatible with my MCU , I have problem with parts number .What is the meaning by R in (STM32F334 "R" 8 T7) ?There is also same part available with C,K and T and ...

Mitesh by Associate II
  • 1924 Views
  • 3 replies
  • 0 kudos

STM32F429 supported LCD modules

Hi.I got the STM32F429 eval board which comes with a small LCD and a demo on it.I was looking into options for using a better LCD but I can't seem to find any examples with the 32F429 with a better display. Is there a list of supported/popular touch ...

DLabi by Associate
  • 2082 Views
  • 3 replies
  • 0 kudos

SPI Overrun when using the DMA

Hi,I've run into an interesting problem when doing two simultaneous SPI transfers using the DMA.I'm using the STM32F103ZFH6 where I am simultaneously reading a bitstream (in large chunks) from and external SPI flash device and writing in out to anoth...

SK by Associate
  • 5765 Views
  • 6 replies
  • 0 kudos

ADC configuration of STM32F051 controller

Can i configure three different ADC channels using ADC interrupt.If so yes, how can i read my values corresponding to each channel from ADC ISR?I have configured ADC interrupt in such a way that the interrupt triggers after all channel sequence.(Havi...

Amal Babu by Associate III
  • 1534 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.