2020-09-22 8:02 AM
We are using the STM32F746 in combination with an exernal SD-RAM.
The clock rate for the RAM is set to a frequency of 96 MHz.
At radiated emission measurement we are above the limit line at 192MHz (double RAM clock)
Is there a possibility to activate jittering or any other option to reduce the radiated emmisions of the electronic system?
2020-09-22 10:01 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.