2013-04-16 12:57 PM
Hi
My application depends on the discovery board design where I need to record and play simultaneously. It seems when it record only the recorded wave is clear with low noise , but when playing wave at same time the recorded sound is full of noise and not clear . I am debugging for hours but no way .. can it be ?:Any suggestions?
Also I cant open the recorded file rec.wave in windows7 any suggestion here too . Thank you in advanced Esat #stm32f42013-04-16 11:32 PM
I am not an expert in USB, so I can't judge the viability of you design (which code you not revealed).
But to check if you have dropouts, or to measure noise, create a sine signal of reasonable frequency and level, and check the output signal. In case of visible/audible trouble, you can trace it's way back through the code.2013-04-17 2:12 AM
The code depends on the discovery code .. same code ..
I hope one of the discovery board people from ST reply because it is the heart of the design to play and record at same time .. if the stm32f4 cant handle that ( I dont think so ) so I need to change the design to use 2 MCU one for recording and other for playing. Could be a problem in the Mic in case of wrong soldering ?2013-04-17 2:46 AM
I hope one of the discovery board people from ST reply because it is the heart of the design to play and record at same time ..
Could you explain what you mean ? There is no audio/mic input to the STM32F4, at least I can't see any. I understand sect. 4.6 ''On board audio capability'' that you can input audio data (from a mic) to the CS43L22 directly only, bypassing the MCU. Otherwise, the audio DAC is driven by I2S, so I can't see a performance bottleneck in the MCU here. To cite directly:�? The sound can be output in different ways through audio DAC:
– Using I2S protocol – Using the STM32F4 DAC to analog input AIN1x of the CS43L22 – Using the microphone output directly via a low pass filter to analog input AIN4x of the CS43L22
2013-04-17 5:24 AM
Hi FM
There is MEM audio sensor (mic) on the board .. However I guess I found the problem in my board I use speaker output not headphone output . it seems CS43L22 limits the signal and distroy the wave. I am still debugging .. but why I can still open the recorded wave in windows XP not in windows 7 ..2013-04-17 5:53 AM
There is MEM audio sensor (mic) on the board ..
Well, that makes sense. And there shouldn't be a performance problem to drive both at the same time. But perhaps you overload the output, and get clipping ?but why I can still open the recorded wave in windows XP not in windows 7 ..
That seems a different story altogether...
2013-04-18 7:35 AM
Why don't you try to save a chunk of data in the internal buffer and then reproduce it to ensure everything works ok in your code? Forget storage, for now.
Are you acquiring data and reproducing it at the correct sample rate?Toggle a pin in the interrupt routine and then measure the time with an oscilloscope to ensure everything works fine.2013-04-22 1:08 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.