2010-10-20 2:29 AM
hi
i saw that the slower watch dog i can make will reset after /* On Value line devices, Enable WWDG and set counter value to 127, WWDG timeout = ~1366 ×–s * 64 = 87.42 ms */ can i make it slower like 500msec? thanks.2010-10-20 9:18 AM
Use the Independent watchdog (IWDG) it has a 12-bit counter, and an 8-bit prescaler off the 40 KHz LSI. Max timeout is in the order of 26 seconds.
2010-10-20 11:24 PM
hi.
i tried using the IWDG but for some reason it does not work when ever it needs to reset the CSTACK gets full and it does not start. why? #include ''stm32F10x.h'' #define IWDG_WriteAccess_Enable ((uint16_t)0x5555) #define IWDG_Prescaler_32 ((uint8_t)0x03) #define KR_KEY_Reload ((uint16_t)0xAAAA) #define KR_KEY_Enable ((uint16_t)0xCCCC) #define CSR_RMVF_Set ((uint32_t)0x01000000) void setsystemclock(void); void uartfunction(void); uint8_t TxBuffer[] = ''Buffer Send from USART3 to USARTz using Flags''; uint8_t TxCounter = 0, RxCounter = 0; int main(void) { char byte_temp=0; setsystemclock(); //set system clock to 24Mhz RCC->CSR |= CSR_RMVF_Set; //watchdog configuration IWDG->KR=IWDG_WriteAccess_Enable;//unlock WDG registers /* IWDG counter clock: 40KHz(LSI) / 32 = 1.25 KHz */ IWDG->PR =IWDG_Prescaler_32; IWDG->RLR =349;//reload value IWDG->KR =KR_KEY_Reload; //IWDG->KR = KR_KEY_Enable; RCC->APB2ENR =RCC_APB2RSTR_IOPCRST | RCC_APB2RSTR_AFIORST;//port C clock and alternative clock enable. page 79 RCC->APB1ENR =RCC_APB1ENR_USART3EN ; GPIOC->CRH=GPIO_CRH_MODE10 | GPIO_CRH_CNF10_1 | GPIO_CRH_CNF11_0 ;//PC11 in input floating mode for RX. PC10 Alternative Output TX. AFIO->MAPR=AFIO_MAPR_USART3_REMAP_0 ;//port remap as uart //PC10 TX PC11 RX USART3->CR1 =USART_CR1_RE | USART_CR1_TE; //Receiver enable, Transmitter enable, USART disable USART3->BRR=0x9C4;//9600 at 24Mhz USART3->CR1 |= USART_CR1_UE;; //Uart Enable; while (((USART3->SR) & USART_SR_TXE)==0); USART3->DR = 'S'; IWDG->KR = KR_KEY_Enable; while(1) { IWDG->KR =KR_KEY_Reload; if (((USART3->SR)&USART_SR_RXNE)>0) { byte_temp= USART3->DR; if (((USART3->SR)&USART_SR_TXE)>0) { USART3->DR =(byte_temp+1); while(1);//reset here } } /* while(TxCounter < 30) { USART3->DR =('5'); while(((USART3->SR)&USART_SR_TXE)==0);// Loop until USARTy DR register is empty TxCounter++; } TxCounter=0;*/ } } void setsystemclock(void) { RCC->CR |= RCC_CR_HSEON; // Wait until it's ready while ((RCC->CR & RCC_CR_HSERDY) == 0) ; // Select PREDIV1 as PLL source and sett PLL mul to 3 (set bit 0) // for 8*3 = 24 MHz RCC->CFGR |= RCC_CFGR_PLLSRC | RCC_CFGR_PLLMULL_0; // Start PLL RCC->CR |= RCC_CR_PLLON; // Wait until it's ready while ((RCC->CR & RCC_CR_PLLRDY) == 0) ; // Select PLL as system clock RCC->CFGR |= RCC_CFGR_SW_PLL; // Here we can check if PLL is used, and maybe disable HSI // Disable HSI RCC->CR &= ~RCC_CR_HSION; RCC->CFGR|=RCC_CFGR_MCO_2; //sys clock output }2010-10-21 12:00 AM
2010-10-21 12:53 AM
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.