2022-02-16 6:42 AM
I want to wake up from standby for each transition on a wkup pin. For example, on waking, read the wakup pin and set/reset the bit in pwr_cr4. (pin high -> bit high, pin low -> bit low).
Is there a race condition ? The reference manual is vague on the logic behind the wkup pins. The configuration is for detecting an edge. In the example above, changing the edge to be detected based upon the current line state introduces a possible race condition depending upon how the hardware works.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.