2017-06-21 3:55 AM
Hello.
There was a problem with the operation of the ADC with built-in thermistor and VBAT voltage.
The value 4095 is always read.
Here is an example of code for reading voltage VBAT:
/* Configure the ADC clock */
RCC_ADCCLKConfig(RCC_ADC12PLLCLK_Div2); /* Enable ADC1 clock */ RCC_AHBPeriphClockCmd(RCC_AHBPeriph_ADC12, ENABLE); /* Setup SysTick Timer for 1 �sec interrupts */ if (SysTick_Config(SystemCoreClock / 1000000)) { /* Capture error */ while (1) {} } ADC_StructInit(&ADC_InitStructure); /* Calibration procedure */ ADC_VoltageRegulatorCmd(ADC1, ENABLE); /* Insert delay equal to 10 �s */ Delay(10); ADC_SelectCalibrationMode(ADC1, ADC_CalibrationMode_Single); ADC_StartCalibration(ADC1); while(ADC_GetCalibrationStatus(ADC1) != RESET ); calibration_value = ADC_GetCalibrationValue(ADC1); Delay(100); ADC_CommonInitStructure.ADC_Mode = ADC_Mode_Independent; ADC_CommonInitStructure.ADC_Clock = ADC_Clock_AsynClkMode; ADC_CommonInitStructure.ADC_DMAAccessMode = ADC_DMAAccessMode_Disabled; ADC_CommonInitStructure.ADC_DMAMode = ADC_DMAMode_OneShot; ADC_CommonInitStructure.ADC_TwoSamplingDelay = 0; ADC_CommonInit(ADC1, &ADC_CommonInitStructure); ADC_InitStructure.ADC_ContinuousConvMode = ADC_ContinuousConvMode_Disable; ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b; ADC_InitStructure.ADC_ExternalTrigConvEvent = ADC_ExternalTrigConvEvent_0; ADC_InitStructure.ADC_ExternalTrigEventEdge = ADC_ExternalTrigEventEdge_None; ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right; ADC_InitStructure.ADC_OverrunMode = ADC_OverrunMode_Disable; ADC_InitStructure.ADC_AutoInjMode = ADC_AutoInjec_Disable; ADC_InitStructure.ADC_NbrOfRegChannel = 1; ADC_Init(ADC1, &ADC_InitStructure); ADC_RegularChannelConfig(ADC1, ADC_Channel_Vbat, 1, ADC_SampleTime_7Cycles5); ADC_VbatCmd(ADC1, ENABLE); /* Enable ADC1 */ ADC_Cmd(ADC1, ENABLE); /* wait for ADRDY */ while(!ADC_GetFlagStatus(ADC1, ADC_FLAG_RDY)); /* Infinite loop */ while (1) { ADC_StartConversion(ADC1); /* Test EOC flag */ while(ADC_GetFlagStatus(ADC1, ADC_FLAG_EOC) == RESET); /* Get ADC1 converted data */ ADC1ConvertedValue =ADC_GetConversionValue(ADC1); /* Compute the voltage */ ADC1ConvertedVoltage = (ADC1ConvertedValue *3300)/0xFFF; printf('ADC1ConvertedValue = %d\r\n',ADC1ConvertedValue); }Reading the temperature sensor is similar, only the ADC channel selection differs:
ADC_RegularChannelConfig(ADC1, ADC_Channel_TempSensor, 1, ADC_SampleTime_7Cycles5);
ADC_TempSensorCmd(ADC1, ENABLE);In both cases, the ADC returns a value of 4095.
What am I doing wrong?
In the attachment - the whole project:
adc_std_01.rar -
VBAT measurement design
adc_std_02.rar -
Temperature measurement project
adc_01.rar -
A temperature measurement project assembled in CubeMX using HAL
adc_02.rar -
VBAT measurement design, assembled in CubeMX using HAL
Thanks in advance.
#temperature-sensor #stm32f303 #stm32f303-adc #vbat-monitoring2017-07-14 1:46 AM
I currently have the same problem with the internal temperature sensor of STM32F303VBT6 (using Cube 4.21.0 and FW-lib 1.8.0). Always get value 4095. Same approach on STM32F302 works fine.
2017-07-14 2:24 AM
Hello Serhii and Daniel
What is your harware configuration about VDDA and VSSA pins ?
Is VDDA-VSSA voltage higher(according ofcourse to the RM) than the voltage try to read?
In case this voltagedifference between theese two power pins is less than the voltage you try to read (and VSSA have some connection with ground), the value 4095 (12 bits full reading) is normal.
Look at RM0316 page 310 about theese pins.
2017-07-18 9:21 AM
Hi Vangelis,
yes, that was the problem. On the layout for STM32F303 VREF+ was not connected. On STM32F302 VDDA and VREF+ share one µC pin. Thx!
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.