2025-08-14 6:32 AM
Hi everyone,
I’m looking for the latest condition-based predictive maintenance kits or devices with the following features:
1. Vibration monitoring
2. Acoustic sensing
3. Temperature monitoring
4. Battery Powered, Low Voltage
5. Wi-Fi connectivity
6. AI-based anomaly detection/failure prediction
7. Cloud connectivity.
Could you please let me know the latest and best recommended product that meets these requirements? Any details on specs, AI capabilities, and cloud integration would be greatly appreciated.
Thanks!
Sajid
Solved! Go to Solution.
2026-01-03 3:43 AM
I completed the Wi-Fi implementation using the STWINBX1_WIFI demo code provided by ST.
2025-08-17 3:38 AM - edited 2025-08-17 3:40 AM
Hi again,
I’ve studied the technical specifications of the following ST kits for my use case (condition-based predictive maintenance with vibration, acoustics, temperature, battery power, Wi-Fi, edge-AI anomaly detection, and cloud connectivity):
STEVAL-PROTEUS1
STEVAL-STWINBX1 (STWIN.box)
STEVAL-STWINKT1
STEVAL-MKSBOX1V1 (SensorTile.box)
STEVAL-STWINKT1B
From this analysis, STEVAL-STWINBX1 looks to be the most suitable overall (sensing coverage, battery operation, BLE/Wi-Fi, and support for embedded AI + cloud).
This is for my Master’s final project, and I will probably be using Azure IoT Cloud for the cloud integration.
Question: Is there a newer or more advanced ST kit/device than STWIN.box for this type of application—for example, a next-gen platform with improved wide-band vibration + ultrasound capture, low-power Wi-Fi, enhanced on-board ML/TrustZone, or out-of-the-box cloud reference integrations?
If there’s a recommended successor/roadmap product (or specific expansion boards/firmware packs) I should look at, I’d greatly appreciate your advice.
Thanks!
Sajid
2025-10-04 6:04 AM - last edited on 2025-10-04 9:04 AM by Andrew Neil
Hello, I have recently purchased the STEVAL-STWINBX1 board, and I’m exploring it for predictive maintenance applications. I’m aware that FP-AI-PREDMNT2 + DSH-PREDMNT are available for the STEVAL-STWINKT1B kit. Could anyone let me know if there is a cloud application/dashboard package (like DSH-PREDMNT) officially available or supported for the STWINBX1 as well?
See separate thread for the new dashboard question: STEVAL-STWINBX1 – Cloud Dashboard (DSH-PREDMNT) for Predictive Maintenance ?
2026-01-03 3:43 AM
I completed the Wi-Fi implementation using the STWINBX1_WIFI demo code provided by ST.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.