2016-02-28 4:43 AM
Hi.
I would like to understand wheather it is possible to use the FSMC of the STM32F439 to interface with a MCP module - NOR FLASH+pSRAM, where the address and data are shared and multiplexed . I see that there is a bank for NOR /PSRAM , but is it possible to work with both on the same chip ? will it be possible to boot from the nor and run with the RAM after ? does the driver support address/data multiplexing ? thank you ! Daniel2016-02-28 5:09 AM
Well ''booting'' from external memory is problematic because you need something to configure the pins, buses, and settings, which are part/board specific.
In the STM32 you'd need to have some minimal code in FLASH which brings up the interfaces in the desired fashion, and then transfers control.We’re moving the ST Community to a new platform to give you a better and more reliable community experience.