STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Which DMA-Channels for simple Audio (Mono ADC/DAC)?

Posted on February 27, 2016 at 12:58Hi, could somebody recommend me perhaps, which DMA configuration to use for simple Audio (STM32L4, Analog micro connected to ADC, simple speaker amp connected to DAC - I want do record to WAV files and play back f...

flyer31 by Senior
  • 1495 Views
  • 2 replies
  • 0 kudos

STM32F072-DISCO UART DMA doesn't work

Posted on February 20, 2016 at 18:28Code is in the Attatchments.I'm trying to periodically send data over SPI and to receive data over USART. Sending over SPI w/ DMA works. But the USART DMA doesn't work. I can send whichever data I want, but the DM...

Leonelf by Associate II
  • 4291 Views
  • 5 replies
  • 0 kudos

SPI - RXNE not updating in debugger mode

Posted on February 27, 2016 at 20:04 Hi, I am pasting a piece of code I used for SPI communication in STM32F4 Discovery board.The code is working, I have no doubts. I faced an issue while in debugger mode. I added a break point at l...

STM32F429-Discovery, 70kB array into flash

Posted on February 27, 2016 at 16:59Hi.I would like to play audio wav (mono, 8kHz, 8 bit) file using DAC. I took 10 sec of some record and converted it to wav file with above parameters. The achieved file is about 70kB.I made a hex file with an arra...

baev_al by Associate III
  • 1624 Views
  • 5 replies
  • 0 kudos

STM32F4xx HAL SPI Driver V1.4.4

Posted on February 20, 2016 at 07:18This release has the following note and I haven't been able to figure out why there is this limitation and am hoping some here can help. Add note to the max frequencies reached in all modes.Add note about Master...

Crash

Posted on February 26, 2016 at 11:34HiCould anyone tell me, how to check the cause of crash ?..

arunease by Associate II
  • 1004 Views
  • 2 replies
  • 0 kudos

stm32cube dont start from MDK5

Posted on February 27, 2016 at 01:00helloi am trying to configure a project for stm32f205vft6, o i start a new project inMDK5 and i want to use the stm32cubemx as framework.but when MDK5 ask to press yes to start the stm32cubemx , this window isdisp...

websat13 by Associate II
  • 952 Views
  • 0 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.