2016-02-23 8:44 AM
Hello,
i'm using cubeMx 4.13.0. Sometimes the user constants are erased when using CubeMx. I attached a project. To reproduce the problem you just have to :- open the project- go to Configuration- enter the timer 1- exit timer 1 configuration without modification (cancel)- go to pinout- go to Configuration again, there are red crosses on timer 1 and 6. The user constants have been erased.Is there a work around ?Thanks.Philippe2016-02-23 11:54 PM
Hello Philippe,
Thank you for reporting this issue. The sole workaround for now is to avoid using the cancel button. We shall fix this a.s.a.p. in next CubeMX release. Best regards2016-03-22 11:18 AM
Dear user,
this is fixed in STM32CubeMX 4.14We’re moving the ST Community to a new platform to give you a better and more reliable community experience.