STM32 MCUs Products

Ask questions, find answers, and share insights on STM32 products and their technical features.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

[Bug] STM32Cube - HardFault handler has wrong name

Posted on January 17, 2016 at 17:37 Hello I'd like to report a bug with the current version of STM32CubeMX 4.0 and the F4 libraries 1.1 concerning the code generation. Currently if the user enables the hard fault interrupt the ge...

STM32CubeMX Standard I2S Frequencies

Posted on January 18, 2016 at 16:05I need to use a standard I2S audio sample rate that is different than the ones in the list provided by STM32CubeMX.  There are many hardware and software codecs that support 12KHz and 24KHz, which are not included ...

kevin2399 by Associate III
  • 1483 Views
  • 3 replies
  • 0 kudos

User constants lost

Posted on February 23, 2016 at 17:44Hello,i'm using cubeMx 4.13.0. Sometimes the user constants are erased when using CubeMx. I attached a project. To reproduce the problem you just have to :- open the project- go to Configuration- enter the timer 1...

cubemx 4.13.0 STM32F4 what's wrong with SPI RX DMA?

Posted on February 29, 2016 at 14:46 Hello! After upgrading to latest version of cubemx (to 4.0) and updating HAL library to v1.0 my SPI code is broken in strage way - NSS pin state is igneored! My test setup: STM32F429VGT6 168 ...

l-proger by Associate III
  • 2082 Views
  • 3 replies
  • 0 kudos

STM32CubeMX V4.13.0 problems

Posted on February 07, 2016 at 04:30Yesterday I upgraded to V4.13.0 which required that I also upgrade to STM32CubeL4 V1.3.0.Since then, every project that I generate exhibits a couple of problems:1) every reference to RCC_xxx #defines shows up in t...

STM32CubeMX for Nucleo-L476-RG base project

Posted on March 15, 2016 at 14:58Dear All.I�ve recently installed STM32Cube MX 4.13.0 on both Ubuntu 14 and Windows 10, with the purpose of generating base code for my Nucleo-L476-RG equipped with MEMS sensors daughterboards.I use SW4STM32 fully upd...

Debugger starts up at wrong address.. sometimes..

Posted on March 22, 2016 at 17:39Hi All, I just started working on a STM32L151. I've setup the debugger to break at first instruction (not main), but when I start debugging the program counter stops at 0x1ff00b84 which isn't even a part of the flash...

texton1 by Associate II
  • 2086 Views
  • 2 replies
  • 0 kudos

STM32CubeMX projects are not work in TrueStudio

Posted on January 19, 2016 at 13:12HiI just made a STM32FCubeMX projects for TrueStudio.But, always compile error.The error message is C:\Users\sohae\Desktop\save\STM32F411BASE\TrueSTUDIO\STM32F411BASE Configuration\Debug/..\..\..\Drivers\CMSIS\Devi...

Auto baud rate detection for UART

Posted on March 16, 2016 at 23:40Hi.I would like to implement auto baud rate detection for UART in STM32F303 uC. There are 4 different detection modes. I understand how each of them works (what is being measured), but don't know, if any of that mode...

matic by Associate III
  • 890 Views
  • 1 replies
  • 0 kudos

FMC

Posted on March 22, 2016 at 13:48

arunease by Associate II
  • 690 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.