2016-12-05 7:13 PM
I want to create the USB HID device function but I don't have any library or example code.
Where to download the relation data for me reference?PS:I use a STM32F427 MCU.2016-12-06 12:14 AM
Dear
Chen.Pohua
,
To have more insight into the USB HID using the STM32Cube library, you can review the USB libraries and start from USB HID examples within the :STM32Cube_FW_F4_V1.0\Projects\STM324xG_EVAL\Applications\USB_Device
You can refer also to the following documents: : STM32Cube™ USB host library : STM32Cube™ USB device libraryBest Regards
-Imen-
2016-12-06 12:34 AM
Hello
You can look on this presentation labs. They are little older but there is described how to create the HID device with CubeMX
Best regards
Radek
2016-12-11 8:00 PM
Dear Imen and Radek:
Thank you for your reply but I don't have an idea to develop my USB HID device because I use a standalone method to create my FW.I have referenced the STM32_USB-Host-Device_Lib_V2.2.0\Project\USB_Device_Examples\HID\src\usbd_desc, but I confuse the the descriptor doesn't include the descriptor description as configuration_descriptor, interface_descriptor, class_descriptor, endpoint_descriptor and HID Report descriptor.
So I don't know how to create my HID device and the host can emulate the F427 to standard USB HID device?
Do you have some examples for my reference?
Thanks!
Best Regards
PohuaWe’re moving the ST Community to a new platform to give you a better and more reliable community experience.