2017-02-20 1:39 PM
Hello all,
I'm trying to configure USART on a STM32F101RB micrcontroller with Atollic True Studio.
the uC clock is configured as external clock (8Mhz) divided by 2 and pll'ed by 9 to a total 36Mhz.
I'm using the HAL to initialize the microcontroller, but so far I hadn't had success. I know the hw is working ok because setting that port with mikroC... it works.
normal usart initialization
static void MX_USART2_UART_Init(void){
huart2.Instance = USART2;
huart2.Init.BaudRate = 115200; huart2.Init.WordLength = UART_WORDLENGTH_8B; huart2.Init.StopBits = UART_STOPBITS_1; huart2.Init.Parity = UART_PARITY_NONE; huart2.Init.Mode = UART_MODE_TX_RX; huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE; huart2.Init.OverSampling = UART_OVERSAMPLING_16; if (HAL_UART_Init(&huart2) != HAL_OK) { Error_Handler(); }}Clock for porta has already been enabled by calling:
__HAL_RCC_GPIOA_CLK_ENABLE();
and finally the Hw initialization is as follows:
void HAL_UART_MspInit(UART_HandleTypeDef* huart){
GPIO_InitTypeDef GPIO_InitStruct;
if(huart->Instance==USART2){ __HAL_RCC_AFIO_CLK_ENABLE();AFIO->MAPR &= (~AFIO_MAPR_USART2_REMAP_Msk);
__HAL_RCC_USART2_CLK_ENABLE();
/**USART2 GPIO Configuration
PA2 ------> USART2_TX PA3 ------> USART2_RX */ GPIO_InitStruct.Pin = GPIO_PIN_2; GPIO_InitStruct.Mode = GPIO_MODE_AF_PP; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_HIGH; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);GPIO_InitStruct.Pin = GPIO_PIN_3;
GPIO_InitStruct.Mode = GPIO_MODE_INPUT; GPIO_InitStruct.Pull = GPIO_NOPULL; HAL_GPIO_Init(GPIOA, &GPIO_InitStruct); }}
with this I've tryed to send the eternal 'Hello World' as follows:
while(1){
char msg[] = 'Hello World!\n\r';
HAL_UART_Transmit(&huart2, (uint8_t*)msg, strlen(msg), 0xFFFF);}
but no success, I've even checked if alternative pins were enabled, but, they were not.
any ideas of what can be wrong?
thanks in advanced,
Best regards Mauro.#stm32f1012017-02-20 2:15 PM
Have you confirmed the USART2 registers in a debugger? Is the clock enabled?
Do you have a schematic for this hardware? Can you show the working Mikroe C code?
2017-02-20 2:22 PM
Hello Clive One,
thank you for your reply, I haven't check the registers with the debugger, I assumed they were filled correctly after my initialization.
The clock is enabled for PORTA, AFIO, USART2 must I enable the clock for something else?
the Mikroe code is simply the following (only the M letter being sent):
void main() {
while(1){
UART2_Init(115200);
UART2_Write('M');
Delay_ms(1000); /* One second pause */
}}
Best regards, Mauro.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.