2017-02-19 5:23 PM
Ever since the dawn of HAL, every HAL library I have tried has contained compiler detected errors. My latest frustration source is the STM32L4xx HAL library version 1.6.0. The problems are diverse and include:
Some of the problems I can fix myself, but I don’t think I should have to. The root problem seems to be incomplete or non-existent library compile and fix before release.
It’s tough to get universal HAL acceptance with stuff like this going on.
Hal
2017-02-20 2:57 AM
Hi
Baird.Hal
,Could you please provide more detailsabout the issue that you have encountered using the
STM32L4xx HAL library version 1.6.0, so that it will be easier to check and report internally?
-Nesrine-
2017-02-20 6:58 AM
The issue is simple - the libraries need to be compiled and all compiler detected errors fixed before release.
2017-02-20 1:33 PM
My apologies.
I had updated the HAL Peripheral Library, but the device header file stm32L476xx.h was a previous version. I get a clean compile now.
Hal
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.